Door Lock#

The Z-Wave certified Door Lock application shows a lock implementation. It supports user codes to open a door and thereby eliminate the need for traditional keys. It is possible to both lock and unlock the door remotely through the Z-Wave protocol.

The Door Lock application is based on:

Role Type

Listening Sleeping End device (LSS / FLiRS)

Supporting Device Type

Actuator

Device Type

Lock

Generic Type

Entry Control

Specific Type

Door Lock

Requested security keys

S0 and S2_ACCESS
The Door Lock features depend on the security level

The application will only work when securely added to a network by a controller supporting security. The controller MUST support security S2_Access_Control or S0 in order to be able to control the door lock.

Not implemented Door lock functionality:

  • Timed Operation mode

  • Door Lock condition

  • Inside Door Handle State

  • Functionality handling Lock timeout

  • Target mode

  • Auto-Relock, Hold And Release, Block to Block, and Twist Assist

Supported Command Classes#

The Door Lock application implements mandatory and some optional command classes. The table below lists the supported Command Classes, their version, and their required Security class, if any.

Command Class

Version

Required Security Class

Association

2

S0 or Access Control

Association Group Info

3

S0 or Access Control

Basic

2

S0 or Access Control

Battery

1

S0 or Access Control

Device Reset Locally

1

S0 or Access Control

Door Lock

4

S0 or Access Control

Firmware Update Meta Data

5

S0 or Access Control

Indicator

3

S0 or Access Control

Manufacturer Specific

2

S0 or Access Control

Multi-Channel Association

3

S0 or Access Control

Powerlevel

1

S0 or Access Control

Security 0

1

None

Security 2

1

None

Supervision

1

None

Transport Service

2

None

User Code

1

S0 or Access Control

User Credential*

1

S0 or Access Control

Version

3

S0 or Access Control

Z-Wave Plus Info

2

None

*: The User Credential Command Class is only available on specific boards. See the section User Credential Command Class.

User Credential Command Class#

The User Credential Command Class is enabled by default on the following boards:

  • BRD2705A

  • BRD4400B

  • BRD4400C

  • BRD4401B

  • BRD4401C

Support for this command class can be disabled if the User Code Command Class is sufficient, by disabling the User Credential Command Class component.

To enable this command class on other boards, due to flash memory constraints, it is recommended to first disable the Z-Wave CLI Common component before enabling the User Credential Command Class component.

The default credentials are created when the inclusion process finishes.

  • If the User Code Command Class is enabled:

    • User Code 1 is created with a value of 3494.

  • If the User Credential Command Class is enabled:

    • A Programming User with the unique identifier 1, called "Admin" is created.

    • A PIN Code associated with user 1 is created with a value of 3494.

To operate the door bolt with the default credentials, the end device must first be included in a Z-Wave network.

Basic Command Class mapping#

The Basic Command Class is mapped according to the table below.

Basic Command

Mapped Command

Basic Set (Value)

Door Lock Operation Set (Door Lock Mode)

Basic Report (Current Value = 0x00)

Door Lock Operation Report (Door Lock Mode = 0x00)

Basic Report (Current Value = 0xFF)

Door Lock Operation Report (Door Lock Mode = 0xFF)

Association Groups#

The table below shows the available association groups, including supported command classes for Z-Wave and Z-Wave Long Range respectively.

ID

Name

Node Count

Description

1

Lifeline

X

Supports the following command classes:

  • Device Reset Locally: triggered upon reset.

  • Battery: Triggered upon low battery.

  • Door Lock: Triggered upon a change in door lock configuration.

  • Door Lock: Triggered upon a change in door lock operation.

  • Indicator Report: Triggered when LED0 changes state.

  • User Code: Triggered when a user code record is modified.

  • User Credential*: Triggered when a Duress User enters a Credential.

X: For Z-Wave node count is equal to 5 and for Z-Wave Long Range it is 1.\ *: The User Credential Command Class is only available on specific boards. See the section User Credential Command Class.

Usage of Buttons and LED Status#

We are differentiating four different types of button presses. The following types are the same for the BTN0 and BTN1 on the WSTK board. The duration values can be configured under the config directory in app_button_press_config.h file in each generated application/project.

Please note external wakeup is not supported on button 1 in case of brd2603a and brd2603b.

Press Type

Duration

Short Press

0 - 400 ms

Medium Press

401 - 1500 ms

Long Press

1501 - 5000 ms

Very Long Press

Every press longer than Long Press

Button

Action

Description

RST

Press

Resets the firmware of an application (like losing power). All volatile memory will be cleared.

BTN0

Short Press

Simulates entering a PIN Code on a keypad via the User Credential API.
The entered PIN Code is hard-coded with the value of 3494.
A valid Credential entry (i.e., button press) toggles the Door Lock Mode between Secured and Unsecured, with a delay of 2 seconds, to simulate timed hardware operation.
If Credential data for User UID 1, Slot 1 is changed to something other than the default PIN Code, the Door Lock Mode can no longer be toggled by pressing this button.

Medium Press

Sends Battery Report

Long Press

Changes the outside door handle mode to active if it was inactive and vice versa.

BTN1

Short Press

Enter "learn mode" (sending node info frame) to add/remove the device.
Removing the device from a network will reset it.

Very Long Press

Perform a reset to factory default operation of the device, and a Device Reset Locally Notification Command is sent via Lifeline.

LED

Functionality

Description

LED0

Indicator:

Blinks with 1 Hz when learn mode is active.
Used for Indicator Command Class.

LED1

Bolt:

  • Led off -> bolt unlocked

  • Led on -> bolt locked

Firmware Update#

This section will describe backward compatibility when upgrading the Door Lock application from one SDK to a newer version.

CLI Support#

In case CLI support is needed, please install zw_cli_common component to the project. Please note that the zw_cli_common component will modify the power consumption for every application.

The default baud rate is 9600, which allows the underlying EUSART module to work in EM2. On some development kits (e.g. BRD2603A and BRD2705A), the following command should be applied in Simplicity Studio via the Admin console to adjust the baudrate: serial vcom config speed 9600.

Available CLI commands#

Command

Arguments

Description

help

-

Printing all supported CLI commands and their description.

set_learn_mode

-

Toggling the learn mode functionality. In case the learn mode started, but inclusion does not happen, learn mode will automatically stop after about 30 seconds

factory_reset

-

Executing factory reset

get_dsk

-

Printing out the generated DSK of the device

get_region

-

Printing out the set region of the application

battery_report

-

Sending a battery report

enter_user_code

Your current user code. It must be between 4 and 10 digits.

Entering a minimum 4 digit long user code

set_new_user_code

Your new user code. It must be between 4 and 10 digits.

Setting a new user code wich's lenght must be between 4 and 10 digits

set_doorhandle_state

State of the door handle as string. Possible values are deactivate and activate

Updating the doorhandle state to locked or unlocked

get_doorhandle_state

-

Shows the state of the door handle. Can be "pressed" or "released"

get_doorbolt_state

-

Shows the state of the door bolt. Can be "unlocked" or "locked"

get_doorlatch_state

-

Shows the state of the door latch. Can be "closed" or "open"

User Credential Related CLI commands#

The following commands exist only if User Credential Command class is available. See the section User Credential Command Class.

Command

Arguments

Description

u3c_add_user

  • [string] Name of the user

This command will create a new user in U3C database. The user's UUID will be autogenerated.

u3c_add_credential

  • [uint16] Associated User UID

  • [string] Type of the new credential. Can be "pin" or "password"

  • [uint16] Slot number of the new credential

  • [string] Credential data. E.g. 3494

This command will create a new credential and assign it to an existing user.

u3c_modify_user

  • [uint16] User UID to modify

  • [string] Attribute to modify. Can be "type", "name" or "active"

  • [string] New value of the attribute

This command modifies an attribute of an existing user

u3c_modify_credential

  • [string] Type of the credential. Can be "pin" or "password"

  • [uint16] Slot of the credential

  • [string] Attribute to change. Can be "data", "uuid" or "slot"

  • [string] New value of the attribute

This command modifies an existing credential.

u3c_delete_user

  • [uint16] User UID of an existing user to delete

This command deletes an existing user and all of the assigned credentials.

u3c_delete_credential

  • [string] Type of the credential. Can be "pin" or "password"

  • [uint16] Slot of the credential

This command deletes an existing credential from the database.

u3c_get_user

  • [uint16] User UID of an existing user

This command prints the information of an existing user.

u3c_get_credential

  • [string] Type of the credential. Can be "pin" or "password"

  • [uint16] Slot of the credential

This command prints the information of an existing credential.

u3c_enter_credential

  • [string] Type of the credential. Can be "pin" or "password"

  • [string] Credential data

This command enters an existing credential and validates it.

u3c_credential_learn_start

  • [uint16] Learn target UUID

  • [string] Type of the credential. Can be "pin" or "password"

  • [uint16] Learn target slot

Initiates the Credential Learn process locally.

u3c_credential_learn

  • [string] Credential data. E.g. 3494

Enter credential data for User Credential Learn process