Holds radio parameters.

This is mainly useful for dual PHY and switched radio device (2.4 GHz or SubGHz) to retrieve radio parameters.

Public Attributes#

uint8_t

Public Attribute Documentation#

radioTxPower#

int8_t EmberMultiPhyRadioParameters::radioTxPower

Definition at line 1259 of file stack/include/ember-types.h

radioPage#

uint8_t EmberMultiPhyRadioParameters::radioPage

Definition at line 1260 of file stack/include/ember-types.h

radioChannel#

uint8_t EmberMultiPhyRadioParameters::radioChannel

Definition at line 1261 of file stack/include/ember-types.h