Holds network parameters.

For information about power settings and radio channels, see the technical specification for the RF communication module in your Developer Kit.

Public Attributes#

uint16_t
EmberNodeId
uint32_t

Public Attribute Documentation#

extendedPanId#

uint8_t EmberNetworkParameters::extendedPanId[EXTENDED_PAN_ID_SIZE]

The network's extended PAN identifier.


Definition at line 1214 of file stack/include/ember-types.h

panId#

uint16_t EmberNetworkParameters::panId

The network's PAN identifier.


Definition at line 1216 of file stack/include/ember-types.h

radioTxPower#

int8_t EmberNetworkParameters::radioTxPower

A power setting, in dBm.


Definition at line 1218 of file stack/include/ember-types.h

radioChannel#

uint8_t EmberNetworkParameters::radioChannel

A radio channel. Be sure to specify a channel supported by the radio.


Definition at line 1220 of file stack/include/ember-types.h

joinMethod#

EmberJoinMethod EmberNetworkParameters::joinMethod

Join method: The protocol messages used to establish an initial parent. It is ignored when forming a ZigBee network, or when querying the stack for its network parameters.


Definition at line 1225 of file stack/include/ember-types.h

nwkManagerId#

EmberNodeId EmberNetworkParameters::nwkManagerId

NWK Manager ID. The ID of the network manager in the current network. This may only be set at joining when using EMBER_USE_CONFIGURED_NWK_STATE as the join method.


Definition at line 1231 of file stack/include/ember-types.h

nwkUpdateId#

uint8_t EmberNetworkParameters::nwkUpdateId

An NWK Update ID. The value of the ZigBee nwkUpdateId known by the stack. It is used to determine the newest instance of the network after a PAN ID or channel change. This may only be set at joining when using EMBER_USE_CONFIGURED_NWK_STATE as the join method.


Definition at line 1237 of file stack/include/ember-types.h

channels#

uint32_t EmberNetworkParameters::channels

The NWK channel mask. The list of preferred channels that the NWK manager has told this device to use when searching for the network. This may only be set at joining when using EMBER_USE_CONFIGURED_NWK_STATE as the join method.


Definition at line 1243 of file stack/include/ember-types.h