Silicon Labs
zigbee/6.6/group-network
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
Results 1-5 of 5 for zigbee/6.6/group-network in 0.17 seconds
Advertising and Scanning with LE Coded PHY | Advertising & Scanning | Bluetooth LE | v2.13 | Silicon Labs
https://docs.silabs.com/.../adv-and-scanning-with-le-coded-...
// Bluetooth LE//Version 2.13 // ... You are viewing documentation for version: 2.13 ... Starting in Bluetooth 5, it is possible to offload the advertising data payload onto one of the data ...
Develop a Power-Optimized BLE Design Featuring PRS, ADC, and LDMA | Lab Manuals | Bluetooth LE | v5.0 | Silicon Labs
https://docs.silabs.com/.../develop-power-optimized-ble-design-featuring-prs-adc-l...
... measured, the device will notify all connected devices of the new average voltage through Bluetooth Low Energy. Bluetooth Low Energy# The Bluetooth stack can operate all the way down to EM2.
BLE HID Keyboard | Applications | Bluetooth LE | v2.13 | Silicon Labs
https://docs.silabs.com/.../ble-hid-keybo...
// Bluetooth LE//Version 2.13 // ... Bluetooth SIG defines a HID profile that specifies how a device can support HID services over the Bluetooth LE protocol stack using the Generic Attribute ...
Command Line Interface (CLI) - v3.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../overv...
You are viewing documentation for version: 3.2 | Version History Command Line Interface (CLI) ... Functions can use standard output functions such as printf to write information to ...
ProductMicrocontrollers Resource TypeSoftware API documentation
Bluetooth Advertising Data Basics | Advertising and Scanning | Bluetooth LE | v5.0 | Silicon Labs
https://docs.silabs.com/....
5.0 Bluetooth Advertising Data Basics# Introduction# ... of adopted services Bluetooth API reference manual Bluetooth Core Specification - This is the golden reference, but not that easy to ...
    Results 1-5 of 5 for zigbee/6.6/group-network