Standalone#

Definition of the standalone bootloader interface.

Some functions in this file return an EmberStatus value. See error-def.h for definitions of all EmberStatus return values.

See bootloader-interface-standalone.h for source code.

Functions#

uint16_t

Detects if the standalone bootloader is installed, and if so returns the installed version.

Quits the current application and launches the standalone bootloader (if installed). The function returns an error if the standalone bootloader is not present.

Macros#

#define

Define a numerical value for NO BOOTLOADER mode. In other words, the bootloader should not be run.

#define

Define a numerical value for the normal bootloader mode.

#define

Define a numerical value for the recovery bootloader mode.

Function Documentation#

halGetStandaloneBootloaderVersion#

uint16_t halGetStandaloneBootloaderVersion (void )

Detects if the standalone bootloader is installed, and if so returns the installed version.

Parameters
TypeDirectionArgument NameDescription
voidN/A

A returned version of 0x1234 would indicate version 1.2 build 34

Returns


halLaunchStandaloneBootloader#

EmberStatus halLaunchStandaloneBootloader (uint8_t mode)

Quits the current application and launches the standalone bootloader (if installed). The function returns an error if the standalone bootloader is not present.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Amode

Controls the mode in which the standalone bootloader will run. See the bootloader Application Note for full details. Options are:

Both modes also allow an image transfer to begin via serial xmodem.

Returns


Macro Definition Documentation#

NO_BOOTLOADER_MODE#

#define NO_BOOTLOADER_MODE
Value:
0xFF

Define a numerical value for NO BOOTLOADER mode. In other words, the bootloader should not be run.


STANDALONE_BOOTLOADER_NORMAL_MODE#

#define STANDALONE_BOOTLOADER_NORMAL_MODE
Value:
1

Define a numerical value for the normal bootloader mode.


STANDALONE_BOOTLOADER_RECOVERY_MODE#

#define STANDALONE_BOOTLOADER_RECOVERY_MODE
Value:
0

Define a numerical value for the recovery bootloader mode.