Application#
Defiunition of the application bootloader interface.
Some functions in this file return an EmberStatus value. See error-def.h for definitions of all EmberStatus return values.
See bootloader-interface-app.h for source code.
Functions#
Call this function as part of your application initialization to ensure the storage mechanism is ready to use. Note: some earlier drivers may assert instead of returning an error if initialization fails.
Call this function to get information about the attached storage device and its capabilities.
Call this function when you are done accessing the storage mechanism to ensure that it is returned to its lowest power state.
Call this function once before checking for a valid image to reset the call flag.
Reads the app image out of storage, calculates the total file CRC to verify the image is intact.
Invokes the bootloader to install the application in storage. This function resets the device to start the bootloader code and does not return!
Writes data to the specified raw storage address and length without being restricted to any page size Note: Not all storage implementations support accesses that are not page aligned, refer to the HalEepromInformationType structure for more information. Note: Some storage devices require contents to be erased before new data can be written, and will return an EEPROM_ERR_ERASE_REQUIRED error if write is called on a location that is not already erased. Refer to the HalEepromInformationType structure to see if the attached storage device requires erasing.
Reads data from the specified raw storage address and length without being restricted to any page size Note: Not all storage implementations support accesses that are not page aligned, refer to the HalEepromInformationType structure for more information.
Erases the specified region of the storage device. Note: Most devices require the specified region to be page aligned, and will return an error if an unaligned region is specified. Note: Many devices take an extremely long time to perform an erase operation. When erasing a large region, it may be preferable to make multiple calls to this API so that other application functionality can be performed while the erase is in progress. The halAppBootloaderStorageBusy() API may be used to determine when the last erase operation has completed. Erase timing information can be found in the HalEepromInformationType structure.
Determine if the attached storage device is still busy performing the last operation, such as a write or an erase.
Converts pageToBeRead to an address and the calls storage read function. Note: This function is deprecated. It has been replaced by halAppBootloaderReadRawStorage()
Converts pageToBeWritten to an address and calls the storage write function. Note: This function is deprecated. It has been replaced by halAppBootloaderWriteRawStorage()
Read the application image data from storage.
Returns the application bootloader version.
Returns the recovery image version.
Return a value indicating whether the app bootloader supports IBRs.
Macros#
This is the working unit of data for the app bootloader. We want it as big as possible, but it must be a factor of the NVM page size and fit into a single Zigbee packet. We choose 2^6 = 64 bytes.
This is the working unit of data for the app bootloader. We want it as big as possible, but it must be a factor of the NVM page size and fit into a single Zigbee packet. We choose 2^6 = 64 bytes.
Define a numerical value for checking image validity when calling the image interface functions.
Function Documentation#
halAppBootloaderInit#
uint8_t halAppBootloaderInit (void )
Call this function as part of your application initialization to ensure the storage mechanism is ready to use. Note: some earlier drivers may assert instead of returning an error if initialization fails.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
halAppBootloaderInfo#
const HalEepromInformationType* halAppBootloaderInfo (void )
Call this function to get information about the attached storage device and its capabilities.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
A pointer to a HalEepromInformationType data structure, or NULL if the driver does not support this API
halAppBootloaderShutdown#
void halAppBootloaderShutdown (void )
Call this function when you are done accessing the storage mechanism to ensure that it is returned to its lowest power state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
halAppBootloaderImageIsValidReset#
void halAppBootloaderImageIsValidReset (void )
Call this function once before checking for a valid image to reset the call flag.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
halAppBootloaderImageIsValid#
uint16_t halAppBootloaderImageIsValid (void )
Reads the app image out of storage, calculates the total file CRC to verify the image is intact.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Caller should loop calling this function while it returns BL_IMAGE_IS_VALID_CONTINUE to get final result. This allows caller to service system needs during validation.
Call halAppBootloaderImageIsValidReset() before calling halAppBootloaderImageIsValid() to reset the call flag.
Here is an example application call:
halAppBootloaderImageIsValidReset();
while ( (pages = halAppBootloaderImageIsValid() ) == BL_IMAGE_IS_VALID_CONTINUE) {
// make app specific calls here, if any
emberTick();
}
Returns
One of the following:
Number of pages in a valid image
0 for an invalid image
BL_IMAGE_IS_VALID_CONTINUE (-1) to continue to iterate for the final result.
halAppBootloaderInstallNewImage#
EmberStatus halAppBootloaderInstallNewImage (void )
Invokes the bootloader to install the application in storage. This function resets the device to start the bootloader code and does not return!
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
halAppBootloaderWriteRawStorage#
uint8_t halAppBootloaderWriteRawStorage (uint32_t address, const uint8_t * data, uint16_t len)
Writes data to the specified raw storage address and length without being restricted to any page size Note: Not all storage implementations support accesses that are not page aligned, refer to the HalEepromInformationType structure for more information. Note: Some storage devices require contents to be erased before new data can be written, and will return an EEPROM_ERR_ERASE_REQUIRED error if write is called on a location that is not already erased. Refer to the HalEepromInformationType structure to see if the attached storage device requires erasing.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | address | Address to start writing data |
| const uint8_t * | N/A | data | A pointer to the buffer of data to write. |
| uint16_t | N/A | len | Length of the data to write |
Returns
halAppBootloaderReadRawStorage#
uint8_t halAppBootloaderReadRawStorage (uint32_t address, uint8_t * data, uint16_t len)
Reads data from the specified raw storage address and length without being restricted to any page size Note: Not all storage implementations support accesses that are not page aligned, refer to the HalEepromInformationType structure for more information.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | address | Address from which to start reading data |
| uint8_t * | N/A | data | A pointer to a buffer where data should be read into |
| uint16_t | N/A | len | Length of the data to read |
Returns
halAppBootloaderEraseRawStorage#
uint8_t halAppBootloaderEraseRawStorage (uint32_t address, uint32_t len)
Erases the specified region of the storage device. Note: Most devices require the specified region to be page aligned, and will return an error if an unaligned region is specified. Note: Many devices take an extremely long time to perform an erase operation. When erasing a large region, it may be preferable to make multiple calls to this API so that other application functionality can be performed while the erase is in progress. The halAppBootloaderStorageBusy() API may be used to determine when the last erase operation has completed. Erase timing information can be found in the HalEepromInformationType structure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | address | Address to start erasing |
| uint32_t | N/A | len | Length of the region to be erased |
Returns
halAppBootloaderStorageBusy#
bool halAppBootloaderStorageBusy (void )
Determine if the attached storage device is still busy performing the last operation, such as a write or an erase.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
true if still busy or false if not.
halAppBootloaderReadDownloadSpace#
uint8_t halAppBootloaderReadDownloadSpace (uint16_t pageToBeRead, uint8_t * destRamBuffer)
Converts pageToBeRead to an address and the calls storage read function. Note: This function is deprecated. It has been replaced by halAppBootloaderReadRawStorage()
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | pageToBeRead | pass in the page to be read. This will be converted to the appropriate address. Pages are EEPROM_PAGE_SIZE long. |
| uint8_t * | N/A | destRamBuffer | a pointer to the buffer to write to. |
Returns
halAppBootloaderWriteDownloadSpace#
uint8_t halAppBootloaderWriteDownloadSpace (uint16_t pageToBeWritten, uint8_t * RamPtr)
Converts pageToBeWritten to an address and calls the storage write function. Note: This function is deprecated. It has been replaced by halAppBootloaderWriteRawStorage()
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | pageToBeWritten | pass in the page to be written. This will be converted to the appropriate address. Pages are EEPROM_PAGE_SIZE long. |
| uint8_t * | N/A | RamPtr | a pointer to the data to be written. |
Returns
halAppBootloaderGetImageData#
uint8_t halAppBootloaderGetImageData (uint32_t * timestamp, uint8_t * userData)
Read the application image data from storage.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t * | N/A | timestamp | write the image timestamp to this data pointer. |
| uint8_t * | N/A | userData | write the user data field to this buffer. |
Returns
halAppBootloaderGetVersion#
uint16_t halAppBootloaderGetVersion (void )
Returns the application bootloader version.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
halAppBootloaderGetRecoveryVersion#
uint16_t halAppBootloaderGetRecoveryVersion (void )
Returns the recovery image version.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
halAppBootloaderSupportsIbr#
bool halAppBootloaderSupportsIbr (void )
Return a value indicating whether the app bootloader supports IBRs.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
true if the app bootloader supports IBRs, false otherwise
Macro Definition Documentation#
BOOTLOADER_SEGMENT_SIZE_LOG2#
#define BOOTLOADER_SEGMENT_SIZE_LOG2Value:
6
This is the working unit of data for the app bootloader. We want it as big as possible, but it must be a factor of the NVM page size and fit into a single Zigbee packet. We choose 2^6 = 64 bytes.
BOOTLOADER_SEGMENT_SIZE#
#define BOOTLOADER_SEGMENT_SIZEValue:
(1 << BOOTLOADER_SEGMENT_SIZE_LOG2)
This is the working unit of data for the app bootloader. We want it as big as possible, but it must be a factor of the NVM page size and fit into a single Zigbee packet. We choose 2^6 = 64 bytes.
BL_IMAGE_IS_VALID_CONTINUE#
#define BL_IMAGE_IS_VALID_CONTINUEValue:
((uint16_t)0xFFFF)
Define a numerical value for checking image validity when calling the image interface functions.