Modules#
Application#
Application bootloader and generic EEPROM Interface.
The file bootloader-eeprom.h defines generic EEPROM parameters.
Changing EEPROM size will change the size of the application image space without changing the size or relative location of the recovery and reserved sections. See eeprom.c for more information on modifying EEPROM functionality.
See bootloader-eeprom.h for source code.
See app-bootloader.h for source code.
EEPROM interaction functions.#
Initialize EEPROM. Note: some earlier drivers may assert instead of returning an error if initialization fails.
Shutdown the EEPROM to conserve power.
Call this function to get information about the external EEPROM and its capabilities.
Return the size of the EEPROM.
Determine if the exernal EEPROM is still busy performing the last operation, such as a write or an erase.
Read from the external EEPROM.
Write to the external EEPROM.
Erases the specified region of the external EEPROM.
The current version of the HalEepromInformationType data structure.
The current version of the HalEepromInformationType data structure.
The current version of the HalEepromInformationType data structure.
The current version of the HalEepromInformationType data structure.
Eeprom capabilites mask that indicates the erase API is supported.
Eeprom capabilites mask that indicates page erasing is required before new data can be written to a device.
Eeprom capabilites mask that indicates that the write routine is blocking on this device.
Eeprom capabilites mask that indicates that the erase routine is blocking on this device.
Eeprom capabilities mask that indicateds that the partEraseTime field of HalEepromInformationType is in seconds instead of the usual millisecondss.
Required Custom Functions#
Drives the app bootloader. If the ::runRecovery parameter is ::true, the recovery mode should be activated, otherwise it should attempt to install an image. This function should not return. It should always exit by resetting the the bootloader.
Drives the app bootloader. If the ::runRecovery parameter is ::true, the recovery mode should be activated, otherwise it should attempt to install an image. This function should not return. It should always exit by resetting the the bootloader.
Drives the app bootloader. If the ::runRecovery parameter is ::true, the recovery mode should be activated, otherwise it should attempt to install an image. This function should not return. It should always exit by resetting the the bootloader.
Available Bootloader Library Functions#
Functions implemented by the bootloader library that may be used by custom functions.
Activates recoveryMode to receive a new image over xmodem.
Processes an image in the external eeprom.
Macros#
Definition of an EEPROM page size, in bytes. This definition is deprecated, and should no longer be used.
Define the location of the first page in EEPROM. This definition is deprecated, and should no longer be used.
Define the location of the image start in EEPROM as a function of the EEPROM_FIRST_PAGE and EEPROM_PAGE_SIZE. This definition is deprecated, and should no longer be used.
Define EEPROM success status.
Define EEPROM error status.
Define EEPROM error mask.
Define EEPROM page boundary error.
Define EEPROM page size error.
Define EEPROM write data error.
Define EEPROM image too large error.
Define EEPROM invalid address error.
Define EEPROM chip initialization error.
Define EEPROM erase required error.
Define EEPROM error for no erase support.
EEPROM interaction functions. Documentation#
halEepromInit#
uint8_t halEepromInit (void )
Initialize EEPROM. Note: some earlier drivers may assert instead of returning an error if initialization fails.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
halEepromShutdown#
void halEepromShutdown (void )
Shutdown the EEPROM to conserve power.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
halEepromInfo#
const HalEepromInformationType* halEepromInfo (void )
Call this function to get information about the external EEPROM and its capabilities.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
The format of this call must not be altered. However, the content can be changed to work with a different device.
Returns
A pointer to a HalEepromInformationType data structure, or NULL if the driver does not support this API
halEepromSize#
uint32_t halEepromSize (void )
Return the size of the EEPROM.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
The format of this call must not be altered. However, the content
can be changed to work with a different device.
Internal use only. No exposure to application
Returns
int32_t size
halEepromBusy#
bool halEepromBusy (void )
Determine if the exernal EEPROM is still busy performing the last operation, such as a write or an erase.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
The format of this call must not be altered. However, the content can be changed to work with a different device.
Returns
true if still busy or false if not.
halEepromRead#
uint8_t halEepromRead (uint32_t address, uint8_t * data, uint16_t len)
Read from the external EEPROM.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | address | The address to start reading from. |
| uint8_t * | N/A | data | A pointer to where read data is stored. |
| uint16_t | N/A | len | The length of data to read. |
This is the standard external EEPROM read function. The format of this call must not be altered. However, the content can be changed to work with a different device. Note: Not all storage implementations support accesses that are not page aligned, refer to the HalEepromInformationType structure for more information.
Returns
halEepromWrite#
uint8_t halEepromWrite (uint32_t address, const uint8_t * data, uint16_t len)
Write to the external EEPROM.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | address | The address to start writing to. |
| const uint8_t * | N/A | data | A pointer to the data to write. |
| uint16_t | N/A | len | The length of data to write. |
This is the standard external EEPROM write function. The format of this call must not be altered. However, the content can be changed to work with a different device. Note: Not all storage implementations support accesses that are not page aligned, refer to the HalEepromInformationType structure for more information. Note: Some storage devices require contents to be erased before new data can be written, and will return an EEPROM_ERR_ERASE_REQUIRED error if write is called on a location that is not already erased. Refer to the HalEepromInformationType structure to see if the attached storage device requires erasing.
Returns
EEPROM_SUCCESS or EEPROM_ERR
halEepromErase#
uint8_t halEepromErase (uint32_t address, uint32_t totalLength)
Erases the specified region of the external EEPROM.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | address | Address to start erasing |
| uint32_t | N/A | totalLength | Length of the region to be erased |
The format of this call must not be altered. However, the content
can be changed to work with a different device.
Note: Most devices require the specified region to be page aligned,
and will return an error if an unaligned region is specified.
Note: Many devices take an extremely long time to perform an erase
operation. When erasing a large region, it may be preferable to
make multiple calls to this API so that other application
functionality can be performed while the erase is in progress.
The ::halEepromBusy() API may be used to determine
when the last erase operation has completed. Erase timing
information can be found in the HalEepromInformationType structure.
Returns
EEPROM_INFO_VERSION#
#define EEPROM_INFO_VERSIONValue:
(0x0202)
The current version of the HalEepromInformationType data structure.
EEPROM_INFO_MAJOR_VERSION#
#define EEPROM_INFO_MAJOR_VERSIONValue:
(0x0200)
The current version of the HalEepromInformationType data structure.
EEPROM_INFO_MAJOR_VERSION_MASK#
#define EEPROM_INFO_MAJOR_VERSION_MASKValue:
(0xFF00)
The current version of the HalEepromInformationType data structure.
EEPROM_INFO_MIN_VERSION_WITH_WORD_SIZE_SUPPORT#
#define EEPROM_INFO_MIN_VERSION_WITH_WORD_SIZE_SUPPORTValue:
0x0102U
The current version of the HalEepromInformationType data structure.
EEPROM_CAPABILITIES_ERASE_SUPPORTED#
#define EEPROM_CAPABILITIES_ERASE_SUPPORTEDValue:
(0x0001U)
Eeprom capabilites mask that indicates the erase API is supported.
EEPROM_CAPABILITIES_PAGE_ERASE_REQD#
#define EEPROM_CAPABILITIES_PAGE_ERASE_REQDValue:
(0x0002U)
Eeprom capabilites mask that indicates page erasing is required before new data can be written to a device.
EEPROM_CAPABILITIES_BLOCKING_WRITE#
#define EEPROM_CAPABILITIES_BLOCKING_WRITEValue:
(0x0004U)
Eeprom capabilites mask that indicates that the write routine is blocking on this device.
EEPROM_CAPABILITIES_BLOCKING_ERASE#
#define EEPROM_CAPABILITIES_BLOCKING_ERASEValue:
(0x0008U)
Eeprom capabilites mask that indicates that the erase routine is blocking on this device.
EEPROM_CAPABILITIES_PART_ERASE_SECONDS#
#define EEPROM_CAPABILITIES_PART_ERASE_SECONDSValue:
(0x0010U)
Eeprom capabilities mask that indicateds that the partEraseTime field of HalEepromInformationType is in seconds instead of the usual millisecondss.
Required Custom Functions Documentation#
bootloaderInit#
void bootloaderInit ( runRecovery)
Drives the app bootloader. If the ::runRecovery parameter is ::true, the recovery mode should be activated, otherwise it should attempt to install an image. This function should not return. It should always exit by resetting the the bootloader.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | runRecovery | If ::true, recover mode is activated. Otherwise, normal image installation is activated. |
bootloaderInitCustom#
void bootloaderInitCustom ( runRecovery)
Drives the app bootloader. If the ::runRecovery parameter is ::true, the recovery mode should be activated, otherwise it should attempt to install an image. This function should not return. It should always exit by resetting the the bootloader.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | runRecovery | If ::true, recover mode is activated. Otherwise, normal image installation is activated. |
bootloaderAction#
void bootloaderAction (bool runRecovery)
Drives the app bootloader. If the ::runRecovery parameter is ::true, the recovery mode should be activated, otherwise it should attempt to install an image. This function should not return. It should always exit by resetting the the bootloader.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | runRecovery | If ::true, recover mode is activated. Otherwise, normal image installation is activated. |
Available Bootloader Library Functions Documentation#
recoveryMode#
BL_Status recoveryMode (void )
Activates recoveryMode to receive a new image over xmodem.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
BL_SUCCESS if an image was successfully received.
processImage#
BL_Status processImage (bool install)
Processes an image in the external eeprom.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | install | If ::false, it will simply validate the image without touching main flash. If ::true, the image will be programmed to main flash. |
Returns
BL_SUCCESS if an image was successfully installed/validated
Macro Definition Documentation#
EEPROM_PAGE_SIZE#
#define EEPROM_PAGE_SIZEValue:
(128ul)
Definition of an EEPROM page size, in bytes. This definition is deprecated, and should no longer be used.
EEPROM_FIRST_PAGE#
#define EEPROM_FIRST_PAGEValue:
(0)
Define the location of the first page in EEPROM. This definition is deprecated, and should no longer be used.
EEPROM_IMAGE_START#
#define EEPROM_IMAGE_STARTValue:
(EEPROM_FIRST_PAGE * EEPROM_PAGE_SIZE)
Define the location of the image start in EEPROM as a function of the EEPROM_FIRST_PAGE and EEPROM_PAGE_SIZE. This definition is deprecated, and should no longer be used.
EEPROM_ERR_INVALID_CHIP#
#define EEPROM_ERR_INVALID_CHIPValue:
0x86U
Define EEPROM chip initialization error.
EEPROM_ERR_ERASE_REQUIRED#
#define EEPROM_ERR_ERASE_REQUIREDValue:
0x87U
Define EEPROM erase required error.
EEPROM_ERR_NO_ERASE_SUPPORT#
#define EEPROM_ERR_NO_ERASE_SUPPORTValue:
0x88U
Define EEPROM error for no erase support.