Application bootloader See Application for detailed documentation.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
#ifndef __APP_BOOTLOADER_H__
#define __APP_BOOTLOADER_H__
void bootloaderInit();
void bootloaderInitCustom();
void bootloaderAction(bool runRecovery);
BL_Status recoveryMode(void);
BL_Status processImage(bool install);
#endif //__APP_BOOTLOADER_H__
Required Custom Functions#
Drives the app bootloader. If the ::runRecovery parameter is ::true, the recovery mode should be activated, otherwise it should attempt to install an image. This function should not return. It should always exit by resetting the the bootloader.
Drives the app bootloader. If the ::runRecovery parameter is ::true, the recovery mode should be activated, otherwise it should attempt to install an image. This function should not return. It should always exit by resetting the the bootloader.
Drives the app bootloader. If the ::runRecovery parameter is ::true, the recovery mode should be activated, otherwise it should attempt to install an image. This function should not return. It should always exit by resetting the the bootloader.
Available Bootloader Library Functions#
Functions implemented by the bootloader library that may be used by custom functions.
Activates recoveryMode to receive a new image over xmodem.
Processes an image in the external eeprom.
Required Custom Functions Documentation#
bootloaderInit#
void bootloaderInit ( runRecovery)
Drives the app bootloader. If the ::runRecovery parameter is ::true, the recovery mode should be activated, otherwise it should attempt to install an image. This function should not return. It should always exit by resetting the the bootloader.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | runRecovery | If ::true, recover mode is activated. Otherwise, normal image installation is activated. |
bootloaderInitCustom#
void bootloaderInitCustom ( runRecovery)
Drives the app bootloader. If the ::runRecovery parameter is ::true, the recovery mode should be activated, otherwise it should attempt to install an image. This function should not return. It should always exit by resetting the the bootloader.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | runRecovery | If ::true, recover mode is activated. Otherwise, normal image installation is activated. |
bootloaderAction#
void bootloaderAction (bool runRecovery)
Drives the app bootloader. If the ::runRecovery parameter is ::true, the recovery mode should be activated, otherwise it should attempt to install an image. This function should not return. It should always exit by resetting the the bootloader.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | runRecovery | If ::true, recover mode is activated. Otherwise, normal image installation is activated. |
Available Bootloader Library Functions Documentation#
recoveryMode#
BL_Status recoveryMode (void )
Activates recoveryMode to receive a new image over xmodem.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
BL_SUCCESS if an image was successfully received.
processImage#
BL_Status processImage (bool install)
Processes an image in the external eeprom.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | install | If ::false, it will simply validate the image without touching main flash. If ::true, the image will be programmed to main flash. |
Returns
BL_SUCCESS if an image was successfully installed/validated