Modules#

GPIO

Serial

Common#

Common bootloader definitions.

See bootloader-common.h for source code.

Bootloader Status Definitions#

These are numerical definitions for the possible bootloader status codes.

#define

Numerical definition for a bootloader status code: Success.

#define

Numerical definition for a bootloader status code: CRC match.

#define

Numerical definition for a bootloader status code: Image flashed.

#define

Numerical definition for a bootloader status code: serial error.

#define

Numerical definition for a bootloader status code: Error mask.

#define

Numerical definition for a bootloader status code: Failed in header state. Header expected.

#define

Numerical definition for a bootloader status code: Failed write/CRC of header.

#define

Numerical definition for a bootloader status code: Failed file CRC.

#define

Numerical definition for a bootloader status code: Unknown tag.

#define

Numerical definition for a bootloader status code: EBL header error.

#define

Numerical definition for a bootloader status code: Trying to flash odd length bytes.

#define

Numerical definition for a bootloader status code: Indexed past end of block buffer.

#define

Numerical definition for a bootloader status code: Attempt to overwrite bootloader flash.

#define

Numerical definition for a bootloader status code: Attempt to overwrite Simulated EEPROM flash.

#define

Numerical definition for a bootloader status code: Flash erase failed.

#define

Numerical definition for a bootloader status code: Flash write failed.

#define

Numerical definition for a bootloader status code: END tag CRC wrong length.

#define

Numerical definition for a bootloader status code: Received data before query request/response.

#define

Numerical definition for a bootloader status code: Invalid length detected.

#define

Numerical definition for a bootloader status code: Problem with tagBuf detected.

#define

Numerical definition for a bootloader status code: processEbl deferred, call again to continue.

#define

Numerical definition for a bootloader status code: A known tag was found in an unexpected location (eg. header tag found after data)

#define

Numerical definition for a bootloader status code: The specified encryption type is unknown to this bootloader.

#define

Numerical definition for a bootloader status code: No valid encryption key found on the device (ie. It's all 0xFF's). Bootloader will not function until this key is set.

#define

Numerical definition for a bootloader status code: Generic error indicating that there was a problem with the encrypted file when decrypting.

#define

Numerical definition for a bootloader status code: Failed IBR crc.

#define

Numerical definition for a bootloader status code: Incorrect IBR version.

#define

Numerical definition for a bootloader status code: Invalid ebl address in IBR.

#define

Numerical definition for a bootloader status code: Incorrect IBR header.

Bootloader State Flags#

These are numerical flags for the possible bootloader states. These values are used in the bootloader code for making the current state more verbose. The flags do not start at 0 so that they can be output via the serial port during debug and easily screened out of normal xmodem traffic which depends only on ACK (0x06) and NAK (0x15).

#define
TIMEOUT 0x16

Bootloader state flag.

#define

Bootloader state flag.

#define

Bootloader state flag.

#define
BLOCKOK 0x19

Bootloader state flag.

#define

Bootloader state flag.

#define

Bootloader state flag.

#define

Bootloader state flag.

#define

Bootloader state flag.

#define

Bootloader state flag: Start Of Header not received.

#define

Bootloader state flag: Sequence of bytes don't match.

#define

Bootloader state flag: CRC High byte failure.

#define

Bootloader state flag: CRC Low byte failure.

#define

Bootloader state flag: Block received out of sequence.

#define

Bootloader state flag: Partial block received.

#define

Bootloader state flag: Duplicate of previous block.

Enumerations#

enum
@0 {
PRIORITIZE_BEACONS_BASED_ON_PARENT_CLASSIFICATION = 0x0001
PRIORITIZE_BEACONS_BASED_ON_TC_CONNECTVITY = 0x0002
TC_CONNECTIVITY = 0x0010
LONG_UPTIME = 0x0020
BAD_PARENT_CONNECTIVITY = 0x0040
EMBER_OUTGOING_MESSAGES = 0x0001
EMBER_INCOMING_MESSAGES = 0x0002
EMBER_RADIO_IS_ON = 0x0004
EMBER_TRANSPORT_ACTIVE = 0x0008
EMBER_APS_LAYER_ACTIVE = 0x0010
EMBER_ASSOCIATING = 0x0020
EMBER_ZLL_TOUCH_LINKING = 0x0040
EMBER_NETWORK_TIMEOUT_REQUEST = 0x0200
EMBER_SEND_ORPHAN_NOTIFICATION = 0x0400
EMBER_MAC_DATA_POLL_SUPER_RETRY = 0x0800
INITIAL = 0x0000
SCAN_FOR_TOUCH_LINK = 0x0001
SCAN_FOR_DEVICE_INFORMATION = 0x0002
SCAN_FOR_IDENTIFY = 0x0004
SCAN_FOR_RESET = 0x0008
TARGET_NETWORK_FOUND = 0x0010
ABORTING_TOUCH_LINK = 0x0020
SCAN_COMPLETE = 0x0040
TOUCH_LINK_TARGET = 0x0080
FORMING_NETWORK = 0x0100
RESETTING_TO_FACTORY_NEW = 0x0200
ADC_REF_INT = 42U
TOKEN_COUNT
COMM_SERIAL = 0x01
COMM_RADIO = 0x02
}

Typedefs#

typedef uint8_t

Define the bootloader status type.

Bootloader Status Definitions Documentation#

BL_SUCCESS#

#define BL_SUCCESS
Value:
0U

Numerical definition for a bootloader status code: Success.


BL_CRC_MATCH#

#define BL_CRC_MATCH
Value:
2U

Numerical definition for a bootloader status code: CRC match.


BL_IMG_FLASHED#

#define BL_IMG_FLASHED
Value:
3U

Numerical definition for a bootloader status code: Image flashed.


BL_ERR#

#define BL_ERR
Value:
1U

Numerical definition for a bootloader status code: serial error.


BL_ERR_MASK#

#define BL_ERR_MASK
Value:
0x40U

Numerical definition for a bootloader status code: Error mask.


BL_ERR_HEADER_EXP#

#define BL_ERR_HEADER_EXP
Value:
0x41U

Numerical definition for a bootloader status code: Failed in header state. Header expected.


BL_ERR_HEADER_WRITE_CRC#

#define BL_ERR_HEADER_WRITE_CRC
Value:
0x42U

Numerical definition for a bootloader status code: Failed write/CRC of header.


BL_ERR_CRC#

#define BL_ERR_CRC
Value:
0x43U

Numerical definition for a bootloader status code: Failed file CRC.


BL_ERR_UNKNOWN_TAG#

#define BL_ERR_UNKNOWN_TAG
Value:
0x44U

Numerical definition for a bootloader status code: Unknown tag.


BL_ERR_SIG#

#define BL_ERR_SIG
Value:
0x45U

Numerical definition for a bootloader status code: EBL header error.


BL_ERR_ODD_LEN#

#define BL_ERR_ODD_LEN
Value:
0x46U

Numerical definition for a bootloader status code: Trying to flash odd length bytes.


BL_ERR_BLOCK_INDEX#

#define BL_ERR_BLOCK_INDEX
Value:
0x47U

Numerical definition for a bootloader status code: Indexed past end of block buffer.


BL_ERR_OVWR_BL#

#define BL_ERR_OVWR_BL
Value:
0x48U

Numerical definition for a bootloader status code: Attempt to overwrite bootloader flash.


BL_ERR_OVWR_SIMEE#

#define BL_ERR_OVWR_SIMEE
Value:
0x49U

Numerical definition for a bootloader status code: Attempt to overwrite Simulated EEPROM flash.


BL_ERR_ERASE_FAIL#

#define BL_ERR_ERASE_FAIL
Value:
0x4AU

Numerical definition for a bootloader status code: Flash erase failed.


BL_ERR_WRITE_FAIL#

#define BL_ERR_WRITE_FAIL
Value:
0x4BU

Numerical definition for a bootloader status code: Flash write failed.


BL_ERR_CRC_LEN#

#define BL_ERR_CRC_LEN
Value:
0x4CU

Numerical definition for a bootloader status code: END tag CRC wrong length.


BL_ERR_NO_QUERY#

#define BL_ERR_NO_QUERY
Value:
0X4DU

Numerical definition for a bootloader status code: Received data before query request/response.


BL_ERR_BAD_LEN#

#define BL_ERR_BAD_LEN
Value:
0x4EU

Numerical definition for a bootloader status code: Invalid length detected.


BL_ERR_TAGBUF#

#define BL_ERR_TAGBUF
Value:
0x4FU

Numerical definition for a bootloader status code: Problem with tagBuf detected.


BL_EBL_CONTINUE#

#define BL_EBL_CONTINUE
Value:
0x50U

Numerical definition for a bootloader status code: processEbl deferred, call again to continue.


BL_ERR_UNEXPECTED_TAG#

#define BL_ERR_UNEXPECTED_TAG
Value:
0x51U

Numerical definition for a bootloader status code: A known tag was found in an unexpected location (eg. header tag found after data)


BL_ERR_UNK_ENC#

#define BL_ERR_UNK_ENC
Value:
0x52U

Numerical definition for a bootloader status code: The specified encryption type is unknown to this bootloader.


BL_ERR_INV_KEY#

#define BL_ERR_INV_KEY
Value:
0x53U

Numerical definition for a bootloader status code: No valid encryption key found on the device (ie. It's all 0xFF's). Bootloader will not function until this key is set.


BL_ERR_ENC#

#define BL_ERR_ENC
Value:
0x54U

Numerical definition for a bootloader status code: Generic error indicating that there was a problem with the encrypted file when decrypting.


BL_IBR_ERR_CRC#

#define BL_IBR_ERR_CRC
Value:
0x55U

Numerical definition for a bootloader status code: Failed IBR crc.


BL_IBR_ERR_VERS#

#define BL_IBR_ERR_VERS
Value:
0x56U

Numerical definition for a bootloader status code: Incorrect IBR version.


BL_IBR_ERR_ADDR#

#define BL_IBR_ERR_ADDR
Value:
0x57U

Numerical definition for a bootloader status code: Invalid ebl address in IBR.


BL_IBR_ERR_HDR#

#define BL_IBR_ERR_HDR
Value:
0x58U

Numerical definition for a bootloader status code: Incorrect IBR header.


Bootloader State Flags Documentation#

TIMEOUT#

#define TIMEOUT
Value:
0x16

Bootloader state flag.


FILEDONE#

#define FILEDONE
Value:
0x17

Bootloader state flag.


FILEABORT#

#define FILEABORT
Value:
0x18

Bootloader state flag.


BLOCKOK#

#define BLOCKOK
Value:
0x19

Bootloader state flag.


QUERYFOUND#

#define QUERYFOUND
Value:
0x1A

Bootloader state flag.


START_TIMEOUT#

#define START_TIMEOUT
Value:
0x1B

Bootloader state flag.


BLOCK_TIMEOUT#

#define BLOCK_TIMEOUT
Value:
0x1C

Bootloader state flag.


BLOCKERR_MASK#

#define BLOCKERR_MASK
Value:
0x20

Bootloader state flag.


BLOCKERR_SOH#

#define BLOCKERR_SOH
Value:
0x21

Bootloader state flag: Start Of Header not received.


BLOCKERR_CHK#

#define BLOCKERR_CHK
Value:
0x22

Bootloader state flag: Sequence of bytes don't match.


BLOCKERR_CRCH#

#define BLOCKERR_CRCH
Value:
0x23

Bootloader state flag: CRC High byte failure.


BLOCKERR_CRCL#

#define BLOCKERR_CRCL
Value:
0x24

Bootloader state flag: CRC Low byte failure.


BLOCKERR_SEQUENCE#

#define BLOCKERR_SEQUENCE
Value:
0x25

Bootloader state flag: Block received out of sequence.


BLOCKERR_PARTIAL#

#define BLOCKERR_PARTIAL
Value:
0x26

Bootloader state flag: Partial block received.


BLOCKERR_DUPLICATE#

#define BLOCKERR_DUPLICATE
Value:
0x27

Bootloader state flag: Duplicate of previous block.


Enumeration Documentation#

@0#

@0
Enumerator
PRIORITIZE_BEACONS_BASED_ON_PARENT_CLASSIFICATION
PRIORITIZE_BEACONS_BASED_ON_TC_CONNECTVITY
TC_CONNECTIVITY
LONG_UPTIME
BAD_PARENT_CONNECTIVITY
EMBER_OUTGOING_MESSAGES

There are messages waiting for transmission.

EMBER_INCOMING_MESSAGES

One or more incoming messages being processed.

EMBER_RADIO_IS_ON

The radio is currently powered on. On sleepy devices, the radio is turned off when not in use. On non-sleepy devices (EMBER_COORDINATOR, EMBER_ROUTER, or EMBER_END_DEVICE), the radio is always on.

EMBER_TRANSPORT_ACTIVE

The transport layer has messages awaiting an ACK.

EMBER_APS_LAYER_ACTIVE

The ZigBee APS layer has messages awaiting an ACK.

EMBER_ASSOCIATING

The node is currently trying to associate with a ZigBee PRO network.

EMBER_ZLL_TOUCH_LINKING

The node is currently touch linking.

EMBER_NETWORK_TIMEOUT_REQUEST

Network Timeout Request Event.

EMBER_SEND_ORPHAN_NOTIFICATION

Sending Orphan Notification Event.

EMBER_MAC_DATA_POLL_SUPER_RETRY

MAC Data Poll Super Retry Event .

INITIAL
SCAN_FOR_TOUCH_LINK
SCAN_FOR_DEVICE_INFORMATION
SCAN_FOR_IDENTIFY
SCAN_FOR_RESET
TARGET_NETWORK_FOUND
ABORTING_TOUCH_LINK
SCAN_COMPLETE
TOUCH_LINK_TARGET
FORMING_NETWORK
RESETTING_TO_FACTORY_NEW
ADC_REF_INT

Internal reference.

TOKEN_COUNT
COMM_SERIAL
COMM_RADIO

Typedef Documentation#

BL_Status#

typedef uint8_t BL_Status

Define the bootloader status type.