This structure defines a variety of information about the attached external EEPROM device.
Public Attribute Documentation#
capabilitiesMask#
uint16_t HalEepromInformationType::capabilitiesMask
A bitmask describing the capabilites of this particular external EEPROM
pageEraseMs#
uint16_t HalEepromInformationType::pageEraseMs
Maximum time it takes to erase a page. (in 1024Hz Milliseconds)
partEraseTime#
uint16_t HalEepromInformationType::partEraseTime
Maximum time it takes to erase the entire part. (in 1024Hz Milliseconds). Can be changed to be in seconds using EEPROM_CAPABILITIES_PART_ERASE_SECONDS
partDescription#
const char* const HalEepromInformationType::partDescription
Pointer to a string describing the attached external EEPROM
wordSizeBytes#
uint8_t HalEepromInformationType::wordSizeBytes
The number of bytes in a word for the external EEPROM