Network Utility Functions#
API and Callbacks for the Network Utility functionality in the Application Framework.
Network Utility Functions description.
API#
Use this function to form a new network using the specified network parameters.
Use this function to associate with the network using the specified network parameters.
Use this function to find an unused PAN id and form a new network.
Use this function to find a joinable network and join it.
Set the current network to that of the given index and adds it to the stack of networks maintained by the framework. Every call to this API must be paired with a subsequent call to emberAfPopNetworkIndex.
Set the current network to the callback network and adds it to the stack of networks maintained by the framework. Every call to this API must be paired with a subsequent call to emberAfPopNetworkIndex.
Set the current network to that of the given endpoint and adds it to the stack of networks maintained by the framework. Every call to this API must be paired with a subsequent call to emberAfPopNetworkIndex.
Remove the topmost network from the stack of networks maintained by the framework and sets the current network to the new topmost network. Every call to this API must be paired with a prior call to emberAfPushNetworkIndex, emberAfPushCallbackNetworkIndex, or emberAfPushEndpointNetworkIndex.
Return the primary endpoint of the given network index or 0xFF if no endpoints belong to the network.emberAfStatus.
Returns the primary endpoint of the current network index or 0xFF if no endpoints belong to the current network.
API Documentation#
emberAfFormNetwork#
EmberStatus emberAfFormNetwork (EmberNetworkParameters *parameters)
Use this function to form a new network using the specified network parameters.
N/A | parameters | Specification of the new network. |
Returns
An ::EmberStatus value that indicates either the successful formation of the new network or the reason that the network formation failed.
2094
of file app/framework/include/af.h
emberAfJoinNetwork#
EmberStatus emberAfJoinNetwork (EmberNetworkParameters *parameters)
Use this function to associate with the network using the specified network parameters.
N/A | parameters | Specification of the network with which the node should associate. |
Returns
An ::EmberStatus value that indicates either that the association process began successfully or the reason for failure.
2104
of file app/framework/include/af.h
emberAfFindUnusedPanIdAndForm#
EmberStatus emberAfFindUnusedPanIdAndForm (void)
Use this function to find an unused PAN id and form a new network.
N/A |
Returns
An ::EmberStatus value that indicates either the process begin successfully or the reason for failure.
2112
of file app/framework/include/af.h
emberAfStartSearchForJoinableNetwork#
EmberStatus emberAfStartSearchForJoinableNetwork (void)
Use this function to find a joinable network and join it.
N/A |
Returns
An ::EmberStatus value that indicates either the process begin successfully or the reason for failure.
2118
of file app/framework/include/af.h
emberAfPushNetworkIndex#
EmberStatus emberAfPushNetworkIndex (uint8_t networkIndex)
Set the current network to that of the given index and adds it to the stack of networks maintained by the framework. Every call to this API must be paired with a subsequent call to emberAfPopNetworkIndex.
N/A | networkIndex |
2129
of file app/framework/include/af.h
emberAfPushCallbackNetworkIndex#
EmberStatus emberAfPushCallbackNetworkIndex (void)
Set the current network to the callback network and adds it to the stack of networks maintained by the framework. Every call to this API must be paired with a subsequent call to emberAfPopNetworkIndex.
N/A |
2135
of file app/framework/include/af.h
emberAfPushEndpointNetworkIndex#
EmberStatus emberAfPushEndpointNetworkIndex (uint8_t endpoint)
Set the current network to that of the given endpoint and adds it to the stack of networks maintained by the framework. Every call to this API must be paired with a subsequent call to emberAfPopNetworkIndex.
N/A | endpoint |
2141
of file app/framework/include/af.h
emberAfPopNetworkIndex#
EmberStatus emberAfPopNetworkIndex (void)
Remove the topmost network from the stack of networks maintained by the framework and sets the current network to the new topmost network. Every call to this API must be paired with a prior call to emberAfPushNetworkIndex, emberAfPushCallbackNetworkIndex, or emberAfPushEndpointNetworkIndex.
N/A |
2149
of file app/framework/include/af.h
emberAfPrimaryEndpointForNetworkIndex#
uint8_t emberAfPrimaryEndpointForNetworkIndex (uint8_t networkIndex)
Return the primary endpoint of the given network index or 0xFF if no endpoints belong to the network.emberAfStatus.
N/A | networkIndex |
2154
of file app/framework/include/af.h
emberAfPrimaryEndpointForCurrentNetworkIndex#
uint8_t emberAfPrimaryEndpointForCurrentNetworkIndex (void)
Returns the primary endpoint of the current network index or 0xFF if no endpoints belong to the current network.
N/A |
2159
of file app/framework/include/af.h