ZigBee Device Object#

See zigbee-device-stack.h for source code.

Functions#

emberNetworkAddressRequest(EmberEUI64 target, bool reportKids, uint8_t childStartIndex)

Request the 16 bit network address of a node whose EUI64 is known.

emberIeeeAddressRequest(EmberNodeId target, bool reportKids, uint8_t childStartIndex, EmberApsOption options)

Request the EUI64 of a node whose 16 bit network address is known.

emberIeeeAddressRequestToTarget(EmberNodeId discoveryNodeId, bool reportKids, uint8_t childStartIndex, EmberApsOption options, EmberNodeId targetNodeIdOfRequest)
emberEnergyScanRequest(EmberNodeId target, uint32_t scanChannels, uint8_t scanDuration, uint16_t scanCount)

Request that an energy scan be performed and its results returned. This request may only be sent by the current network manager and must be unicast, not broadcast.

emberSetNetworkManagerRequest(EmberNodeId networkManager, uint32_t activeChannels)

Broadcast a request to set the identity of the network manager and the active channel mask. The mask is used when scanning for the network after missing a channel update.

emberChannelChangeRequest(uint8_t channel)

Broadcast a request to change the channel. This request may only be sent by the current network manager. A several second delay occurs from receipt of the broadcast to changing the channel to allow time for the broadcast to propagate.

Send a broadcast for a ZDO Device announcement. Normally, it is NOT required to call this as the stack automatically sends a device announcement during joining or rejoining, as per the spec.

Send a broadcast for a ZDO Parent Announcement. Normally, it is NOT required to call this as the stack automatically sends a Parent Announce when a Zigbee Router/Coordinator reboots, is in a joined or authenticated state, and has at least one device.

uint8_t

Provide access to the stack ZDO transaction sequence number for the last request.

Function Documentation#

emberNetworkAddressRequest#

EmberStatus emberNetworkAddressRequest (EmberEUI64 target, bool reportKids, uint8_t childStartIndex)

Request the 16 bit network address of a node whose EUI64 is known.

Parameters
TypeDirectionArgument NameDescription
EmberEUI64N/Atarget

The EUI64 of the node.

boolN/AreportKids

True to request that the target list their children in the response.

uint8_tN/AchildStartIndex

The index of the first child to list in the response. Ignored if reportKids is false.

Returns


Definition at line 45 of file stack/include/zigbee-device-stack.h

emberIeeeAddressRequest#

EmberStatus emberIeeeAddressRequest (EmberNodeId target, bool reportKids, uint8_t childStartIndex, EmberApsOption options)

Request the EUI64 of a node whose 16 bit network address is known.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/Atarget

The network address of the node.

boolN/AreportKids

True to request that the target list their children in the response.

uint8_tN/AchildStartIndex

The index of the first child to list in the response. Ignored if reportKids is false.

EmberApsOptionN/Aoptions

The options to use when sending the request. See emberSendUnicast() for a description.

Returns


Definition at line 65 of file stack/include/zigbee-device-stack.h

emberIeeeAddressRequestToTarget#

EmberStatus emberIeeeAddressRequestToTarget (EmberNodeId discoveryNodeId, bool reportKids, uint8_t childStartIndex, EmberApsOption options, EmberNodeId targetNodeIdOfRequest)
Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AdiscoveryNodeId
boolN/AreportKids
uint8_tN/AchildStartIndex
EmberApsOptionN/Aoptions
EmberNodeIdN/AtargetNodeIdOfRequest

Definition at line 70 of file stack/include/zigbee-device-stack.h

emberEnergyScanRequest#

EmberStatus emberEnergyScanRequest (EmberNodeId target, uint32_t scanChannels, uint8_t scanDuration, uint16_t scanCount)

Request that an energy scan be performed and its results returned. This request may only be sent by the current network manager and must be unicast, not broadcast.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/Atarget

The network address of the node to perform the scan.

uint32_tN/AscanChannels

A mask of the channels to be scanned.

uint8_tN/AscanDuration

How long to scan on each channel. Allowed values are 0..5, with the scan times as specified by 802.15.4 (0 = 31 ms, 1 = 46 ms, 2 = 77 ms, 3 = 138 ms, 4 = 261 ms, 5 = 507 ms).

uint16_tN/AscanCount

The number of scans to be performed on each channel (1 .. 8).

Returns


Definition at line 95 of file stack/include/zigbee-device-stack.h

emberSetNetworkManagerRequest#

EmberStatus emberSetNetworkManagerRequest (EmberNodeId networkManager, uint32_t activeChannels)

Broadcast a request to set the identity of the network manager and the active channel mask. The mask is used when scanning for the network after missing a channel update.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AnetworkManager

The network address of the network manager.

uint32_tN/AactiveChannels

The new active channel mask.

Returns


Definition at line 114 of file stack/include/zigbee-device-stack.h

emberChannelChangeRequest#

EmberStatus emberChannelChangeRequest (uint8_t channel)

Broadcast a request to change the channel. This request may only be sent by the current network manager. A several second delay occurs from receipt of the broadcast to changing the channel to allow time for the broadcast to propagate.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Achannel

The channel to change to.

Returns


Definition at line 138 of file stack/include/zigbee-device-stack.h

emberSendDeviceAnnouncement#

EmberStatus emberSendDeviceAnnouncement (void )

Send a broadcast for a ZDO Device announcement. Normally, it is NOT required to call this as the stack automatically sends a device announcement during joining or rejoining, as per the spec.

Parameters
TypeDirectionArgument NameDescription
voidN/A

May be used to re-send the device announcement.

Returns


Definition at line 157 of file stack/include/zigbee-device-stack.h

emberSendParentAnnouncement#

EmberStatus emberSendParentAnnouncement (void )

Send a broadcast for a ZDO Parent Announcement. Normally, it is NOT required to call this as the stack automatically sends a Parent Announce when a Zigbee Router/Coordinator reboots, is in a joined or authenticated state, and has at least one device.

Parameters
TypeDirectionArgument NameDescription
voidN/A

May be used to re-send the parent announcement.

Returns


Definition at line 170 of file stack/include/zigbee-device-stack.h

emberGetLastStackZigDevRequestSequence#

uint8_t emberGetLastStackZigDevRequestSequence (void )

Provide access to the stack ZDO transaction sequence number for the last request.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • The last stack ZDO transaction sequence number used.


Definition at line 178 of file stack/include/zigbee-device-stack.h