Additional Information Block Option Record Fields. Provides information regarding the record fields from the linked translation table. Typically, a translation table, which contains the generic switch, multi sensor or the compact attribute reporting GPD, needs to populate the information during commissioning and use it to translate the shorter GPDF to the longer ZCL payload.
Public Attributes#
uint8_t
uint8_t
uint8_t
uint8_t
uint16_t
uint16_t
uint8_t
uint8_t
uint16_t
struct EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::@10::@11
uint8_t
uint8_t
struct EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::@10::@12
union EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::@10
Public Attribute Documentation#
totalLengthOfAddInfoBlock#
uint8_t EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::totalLengthOfAddInfoBlock
Total Length of the additional information block
optionSelector#
uint8_t EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::optionSelector
Option selector
reportIdentifier#
uint8_t EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::reportIdentifier
attrOffsetWithinReport#
uint8_t EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::attrOffsetWithinReport
attributeDataType#
uint8_t EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::attributeDataType
attributeOptions#
uint8_t EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::attributeOptions
compactAttr#
struct EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::@10::@11 EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::compactAttr
Compact Attribute Reporting or Multi sensor
contactStatus#
uint8_t EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::contactStatus
Provides button information of the Generic switch for contacts status
contactBitmask#
uint8_t EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::contactBitmask
Provides the bitmask to evaluate the received contact. As a result, the bitmask only depends on the number of contacts of the current GPD.
genericSwitch#
struct EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::@10::@12 EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::genericSwitch
Generic switch information
optionData#
union EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::@10 EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::optionData