Green Power Data Types#
This file defines data types relevant to the Green Power implementation.
See gp-types.h for source code.
Modules#
EmberGpTranslationTableAdditionalInfoBlockOptionRecordField
GP Types#
Green Power Security Level.
Green Power Security Security Key Type.
Green Power Application ID.
GP proxy table entry status.
GP sink table entry status.
GP Sink Type.
CGp Transmit options.
Addressing modes for CGp messages.
Transmit options for DGp messages.
API#
DGp Send.
Gets tx queue head.
Sets maximum limit for number of entries in the tx queue.
Gets the limit set for maximum number of entries in the tx queue.
Gets the number of entries in the tx queue.
Gets an entry from Tx Queue The function searches the tx queue using gpd address pointed by supplied in the input/output argument txQueue and returns the message buffer that currently holding the outgoing gpdf information, returns EMBER_NULL_MESSAGE_BUFFER if not found.
Adds an entry to Tx Queue This function adds an entry along with supplied payload data to the Buffer queue. Returns the buffer handle if success else null message buffer upon failure.
Remove an entry from Tx Queue This function searches and removes the entry provided.
Purges Tx Queue This function purges the tx queue.
Macros#
Mask used in the green power endpoint incoming message handler to pass bidirectional information. Incoming GPDF has rxAfterTx bit set.
Mask to test if transmit queue is available at green power stub layer to hold an outgoing GPDF.
Number of GP sink list entries. Minimum is 2 sink list entries.
The size of the SinkList entries in sink table in form of octet string that has a format of [<1 byte length>, <n bytes for sink groups>].
GP parameters list represented as a macro for GP endpoint incoming message handler and callbacks prototypes.
GP arguments list represented as a macro while calling GP endpoint incoming message handler and callbacks.
GP arguments list with void type cast represented as a macro to be used in callback stubs.
Bit mask for the proxy table ebtry option bit representing in-range bit field.
Maximum number of bytes in a green power commissioning frame excluding 3 bytes for device ID, option and application information fields.
GPD Source ID when requesting channel request.
GPD wildcard Source ID.
GPD Reserved Source ID. Used in maintenance frame.
GPD Reserved Source ID. All addresses between 0xFFFFFFF9 and 0xFFFFFFFE are reserved.
GPD Reserved Source ID. All addresses between 0xFFFFFFF9 and 0xFFFFFFFE are reserved.
Default value for derived group ID when alias is not used.
Tunneling delay constant Dmin_b in milliseconds. Ref green power specification for more information on this constant.
Tunneling delay constant Dmin_u in milliseconds. Ref green power specification for more information on this constant.
Tunneling delay constant Dmax in milliseconds. Ref green power specification for more information on this constant.
GP Types Documentation#
EmberGpSecurityLevel#
EmberGpSecurityLevel
Green Power Security Level.
Enumerator | |
---|---|
EMBER_GP_SECURITY_LEVEL_NONE | |
EMBER_GP_SECURITY_LEVEL_RESERVED | |
EMBER_GP_SECURITY_LEVEL_FC_MIC | |
EMBER_GP_SECURITY_LEVEL_FC_MIC_ENCRYPTED |
179
of file stack/include/gp-types.h
EmberGpKeyType#
EmberGpKeyType
Green Power Security Security Key Type.
Enumerator | |
---|---|
EMBER_GP_SECURITY_KEY_NONE | |
EMBER_GP_SECURITY_KEY_NWK | |
EMBER_GP_SECURITY_KEY_GPD_GROUP | |
EMBER_GP_SECURITY_KEY_NWK_DERIVED | |
EMBER_GP_SECURITY_KEY_GPD_OOB | |
EMBER_GP_SECURITY_KEY_GPD_DERIVED |
198
of file stack/include/gp-types.h
EmberGpApplicationId#
EmberGpApplicationId
Green Power Application ID.
Enumerator | |
---|---|
EMBER_GP_APPLICATION_SOURCE_ID | |
EMBER_GP_APPLICATION_IEEE_ADDRESS |
221
of file stack/include/gp-types.h
EmberGpProxyTableEntryStatus#
EmberGpProxyTableEntryStatus
GP proxy table entry status.
Enumerator | |
---|---|
EMBER_GP_PROXY_TABLE_ENTRY_STATUS_ACTIVE | |
EMBER_GP_PROXY_TABLE_ENTRY_STATUS_UNUSED |
237
of file stack/include/gp-types.h
EmberGpSinkTableEntryStatus#
EmberGpSinkTableEntryStatus
GP sink table entry status.
Enumerator | |
---|---|
EMBER_GP_SINK_TABLE_ENTRY_STATUS_ACTIVE | |
EMBER_GP_SINK_TABLE_ENTRY_STATUS_UNUSED |
257
of file stack/include/gp-types.h
EmberGpSinkType#
EmberGpSinkType
GP Sink Type.
Enumerator | |
---|---|
EMBER_GP_SINK_TYPE_FULL_UNICAST | |
EMBER_GP_SINK_TYPE_D_GROUPCAST | |
EMBER_GP_SINK_TYPE_GROUPCAST | |
EMBER_GP_SINK_TYPE_LW_UNICAST | |
EMBER_GP_SINK_TYPE_UNUSED |
298
of file stack/include/gp-types.h
EmberCGpTxOption#
EmberCGpTxOption
CGp Transmit options.
Enumerator | |
---|---|
EMBER_CGP_TX_OPTION_NONE | |
EMBER_CGP_TX_OPTION_USE_CSMA_CA | |
EMBER_CGP_TX_OPTION_USE_MAC_ACK | |
EMBER_CGP_TX_OPTION_RESERVED |
445
of file stack/include/gp-types.h
EmberCGpAddressMode#
EmberCGpAddressMode
Addressing modes for CGp messages.
Enumerator | |
---|---|
EMBER_CGP_ADDRESS_MODE_NONE | |
EMBER_CGP_ADDRESS_MODE_RESERVED | |
EMBER_CGP_ADDRESS_MODE_SHORT | |
EMBER_CGP_ADDRESS_MODE_EXTENDED |
465
of file stack/include/gp-types.h
EmberDGpTxOption#
EmberDGpTxOption
Transmit options for DGp messages.
Enumerator | |
---|---|
EMBER_DGP_TX_OPTION_NONE | |
EMBER_DGP_TX_OPTION_USE_GP_TX_QUEUE | |
EMBER_DGP_TX_OPTION_USE_CSMA_CA | |
EMBER_DGP_TX_OPTION_USE_MAC_ACK | |
EMBER_DGP_TX_OPTION_FRAME_TYPE_DATA | |
EMBER_DGP_TX_OPTION_FRAME_TYPE_MAINTENANCE | |
EMBER_DGP_TX_OPTION_RESERVED |
507
of file stack/include/gp-types.h
EmberGpSourceId#
typedef uint32_t EmberGpSourceId
32-bit GPD source identifier
169
of file stack/include/gp-types.h
EmberGpSecurityFrameCounter#
typedef uint32_t EmberGpSecurityFrameCounter
32-bit security frame counter
171
of file stack/include/gp-types.h
EmberGpMic#
typedef uint32_t EmberGpMic
32-bit MIC code
173
of file stack/include/gp-types.h
API Documentation#
emberDGpSend#
EmberStatus emberDGpSend (bool action, bool useCca, EmberGpAddress * addr, uint8_t gpdCommandId, uint8_t gpdAsduLength, uint8_t const * gpdAsdu, uint8_t gpepHandle, uint16_t gpTxQueueEntryLifetimeMs)
DGp Send.
N/A | action | Action to add (true) or remove (false) |
N/A | useCca | Use CCA for GPDF transmission. |
N/A | addr | The gpd address EmberGpAddress. |
N/A | gpdCommandId | GPD Command ID |
N/A | gpdAsduLength | ASDU Length. |
N/A | gpdAsdu | The ASDU buffer that holds the outgoing GPDF as payload. |
N/A | gpepHandle | Handle for the asdu. |
N/A | gpTxQueueEntryLifetimeMs | Life time in milliseconds in Tx queue after which it gets cleared. |
This API adds or removes an outgoing GPDF (passed as ASDU) in the GP stub layer. As part of Gp Response command processing by green power client cluster, this API submits a outgoing a channel configuration or a commissioning reply GPDF. Similarly, it is called with appropriate action to clear the Tx queue upon channel request timeout.
Returns
An EmberStatus as status.
749
of file stack/include/gp-types.h
emberGpGetTxQueueHead#
MessageBufferQueue * emberGpGetTxQueueHead (void )
Gets tx queue head.
N/A |
This function gets the head pointer of the tx queue. Note : since it returns a pointer to memory the head, it 'll not be useful on host.
Returns
pointer to head of tx queue MessageBufferQueue
767
of file stack/include/gp-types.h
emberGpSetMaxTxQueueEntry#
void emberGpSetMaxTxQueueEntry (uint16_t maxEntries)
Sets maximum limit for number of entries in the tx queue.
N/A | maxEntries |
This function sets the maximum number of entries the tx queue is supposed to grow.
773
of file stack/include/gp-types.h
emberGetGpMaxTxQListCount#
uint16_t emberGetGpMaxTxQListCount (void )
Gets the limit set for maximum number of entries in the tx queue.
N/A |
This function gets the limit set for the maximum number of entries the tx queue is supposed to hold.
Returns
limit to the maximum number of entries.
781
of file stack/include/gp-types.h
emberGetGpTxQListCount#
uint16_t emberGetGpTxQListCount (void )
Gets the number of entries in the tx queue.
N/A |
This function gets the number of entries present in tx queue.
Returns
number of entries.
789
of file stack/include/gp-types.h
emberGpGetTxQueueEntryFromQueue#
EmberMessageBuffer emberGpGetTxQueueEntryFromQueue (EmberGpTxQueueEntry * txQueue, uint8_t * data, uint16_t * dataLength, uint16_t allocatedDataLength)
Gets an entry from Tx Queue The function searches the tx queue using gpd address pointed by supplied in the input/output argument txQueue and returns the message buffer that currently holding the outgoing gpdf information, returns EMBER_NULL_MESSAGE_BUFFER if not found.
N/A | txQueue | EmberGpTxQueueEntry A pointer to an allocated memory to get a copy of the tx queue entry from the buffer queue. The caller populates the addr field of this parameter which is used as a search key. |
N/A | data | A pointer to an allocated memory to get a copy of the gpd command payload if an entry is found. This can be passed as NULL if payload is not required by caller. |
N/A | dataLength | A pointer to hold the length of the gpd command payload when an entry is found and the data collector is non-NULL. |
N/A | allocatedDataLength | Size in bytes for the allocated memory for the data collector. If this value is smaller compared to length of the data in the queue, no data gets copied out. |
Returns
Buffer EmberMessageBuffer that holds the entry if found, null message buffer if not found.
804
of file stack/include/gp-types.h
emberGpAddGpTxQueueEntryWithPayload#
EmberMessageBuffer emberGpAddGpTxQueueEntryWithPayload (EmberGpTxQueueEntry * txQueue, uint8_t * data, uint16_t dataLength)
Adds an entry to Tx Queue This function adds an entry along with supplied payload data to the Buffer queue. Returns the buffer handle if success else null message buffer upon failure.
N/A | txQueue | EmberGpTxQueueEntry A pointer to an allocated memory holding the entry with all the members of the structure assigned as needed. |
N/A | data | A pointer holding the data payload. Can be supplied as NULL if there is no data payload. |
N/A | dataLength | Length of the data. |
Returns
Buffer EmberMessageBuffer that holds the entry upon success else null message buffer.
817
of file stack/include/gp-types.h
emberGpRemoveFromTxQueue#
bool emberGpRemoveFromTxQueue (EmberGpTxQueueEntry * txQueue)
Remove an entry from Tx Queue This function searches and removes the entry provided.
N/A | txQueue | EmberGpTxQueueEntry A pointer to an allocated memory holding the entry with gpd addr field assigned, which is used as for searching the tx queue. NOTE : Use of wildcard gpd addr (AppId = 0,SrcId = 0xFFFFFFFF) , removes all the entries of the tx queue. |
Returns
True upon success else false.
827
of file stack/include/gp-types.h
emberGpClearTxQueue#
void emberGpClearTxQueue (void )
Purges Tx Queue This function purges the tx queue.
N/A |
833
of file stack/include/gp-types.h
Macro Definition Documentation#
EMBER_GP_BIDIRECTION_INFO_RX_AFTER_TX_MASK#
#define EMBER_GP_BIDIRECTION_INFO_RX_AFTER_TX_MASKValue:
0x01
Mask used in the green power endpoint incoming message handler to pass bidirectional information. Incoming GPDF has rxAfterTx bit set.
35
of file stack/include/gp-types.h
EMBER_GP_BIDIRECTION_INFO_TX_QUEUE_AVAILABLE_MASK#
#define EMBER_GP_BIDIRECTION_INFO_TX_QUEUE_AVAILABLE_MASKValue:
0x02
Mask to test if transmit queue is available at green power stub layer to hold an outgoing GPDF.
40
of file stack/include/gp-types.h
GP_SINK_LIST_ENTRIES#
#define GP_SINK_LIST_ENTRIESValue:
2
Number of GP sink list entries. Minimum is 2 sink list entries.
45
of file stack/include/gp-types.h
GP_SIZE_OF_SINK_LIST_ENTRIES_OCTET_STRING#
#define GP_SIZE_OF_SINK_LIST_ENTRIES_OCTET_STRINGValue:
(1 + (GP_SINK_LIST_ENTRIES * (sizeof(EmberGpSinkGroup))))
The size of the SinkList entries in sink table in form of octet string that has a format of [<1 byte length>, <n bytes for sink groups>].
50
of file stack/include/gp-types.h
GP_PARAMS#
#define GP_PARAMSValue:
GP parameters list represented as a macro for GP endpoint incoming message handler and callbacks prototypes.
55
of file stack/include/gp-types.h
GP_ARGS#
#define GP_ARGSValue:
GP arguments list represented as a macro while calling GP endpoint incoming message handler and callbacks.
74
of file stack/include/gp-types.h
GP_UNUSED_ARGS#
#define GP_UNUSED_ARGSValue:
GP arguments list with void type cast represented as a macro to be used in callback stubs.
93
of file stack/include/gp-types.h
GP_PROXY_TABLE_OPTIONS_IN_RANGE#
#define GP_PROXY_TABLE_OPTIONS_IN_RANGEValue:
(BIT(10))
Bit mask for the proxy table ebtry option bit representing in-range bit field.
112
of file stack/include/gp-types.h
GP_COMMISSIONING_MAX_BYTES#
#define GP_COMMISSIONING_MAX_BYTESValue:
(55 - 3)
Maximum number of bytes in a green power commissioning frame excluding 3 bytes for device ID, option and application information fields.
117
of file stack/include/gp-types.h
GP_GPD_SRC_ID_FOR_CAHNNEL_CONFIG#
#define GP_GPD_SRC_ID_FOR_CAHNNEL_CONFIGValue:
0x00000000
GPD Source ID when requesting channel request.
122
of file stack/include/gp-types.h
GP_GPD_SRC_ID_WILDCARD#
#define GP_GPD_SRC_ID_WILDCARDValue:
0xFFFFFFFF
GPD wildcard Source ID.
127
of file stack/include/gp-types.h
GP_GPD_SRC_ID_RESERVED_0#
#define GP_GPD_SRC_ID_RESERVED_0Value:
0x00000000
GPD Reserved Source ID. Used in maintenance frame.
132
of file stack/include/gp-types.h
GP_GPD_SRC_ID_RESERVED_FFFFFF9#
#define GP_GPD_SRC_ID_RESERVED_FFFFFF9Value:
0xFFFFFFF9
GPD Reserved Source ID. All addresses between 0xFFFFFFF9 and 0xFFFFFFFE are reserved.
137
of file stack/include/gp-types.h
GP_GPD_SRC_ID_RESERVED_FFFFFFE#
#define GP_GPD_SRC_ID_RESERVED_FFFFFFEValue:
0xFFFFFFFE
GPD Reserved Source ID. All addresses between 0xFFFFFFF9 and 0xFFFFFFFE are reserved.
142
of file stack/include/gp-types.h
GP_DERIVED_GROUP_ALIAS_NOT_USED#
#define GP_DERIVED_GROUP_ALIAS_NOT_USEDValue:
0xffff
Default value for derived group ID when alias is not used.
147
of file stack/include/gp-types.h
GP_DMIN_B#
#define GP_DMIN_BValue:
32
Tunneling delay constant Dmin_b in milliseconds. Ref green power specification for more information on this constant.
152
of file stack/include/gp-types.h
GP_DMIN_U#
#define GP_DMIN_UValue:
5
Tunneling delay constant Dmin_u in milliseconds. Ref green power specification for more information on this constant.
157
of file stack/include/gp-types.h
GP_DMAX#
#define GP_DMAXValue:
100
Tunneling delay constant Dmax in milliseconds. Ref green power specification for more information on this constant.
162
of file stack/include/gp-types.h