ZLL On/Off Server#
API and Callbacks for the ZLL On/Off Cluster Server Component.
Silicon Labs implementation of the original Zigbee Light Link profile enhancements to the On/Off server cluster. The component is only intended to assist with debugging, as the implemented callbacks simply parse requests from the Identify client and blink LEDs. Before production, this component should be replaced with code that acts on the requests in an appropriate way. Note that the extensions do not now require Touchlink commissioning to be used, and that the commands may now be required by other device types, such as Lighting and Occupancy.
Modules#
API#
Turn off ZLL extensions.
Turn on ZLL extensions.
Toggle ZLL extensions.
Level control cluster command for ZLL extensions.
API Documentation#
emberAfPluginZllOnOffServerOffZllExtensions#
EmberAfStatus emberAfPluginZllOnOffServerOffZllExtensions (const EmberAfClusterCommand * cmd)
Turn off ZLL extensions.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const EmberAfClusterCommand * | N/A | cmd | pointer to the cluster command struct Ver.: always |
Returns
EmberAfStatus return status
emberAfPluginZllOnOffServerOnZllExtensions#
EmberAfStatus emberAfPluginZllOnOffServerOnZllExtensions (const EmberAfClusterCommand * cmd)
Turn on ZLL extensions.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const EmberAfClusterCommand * | N/A | cmd | pointer to the cluster command struct Ver.: always |
Returns
EmberAfStatus return status
emberAfPluginZllOnOffServerToggleZllExtensions#
EmberAfStatus emberAfPluginZllOnOffServerToggleZllExtensions (const EmberAfClusterCommand * cmd)
Toggle ZLL extensions.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const EmberAfClusterCommand * | N/A | cmd | pointer to the cluster command struct Ver.: always |
Returns
EmberAfStatus return status
emberAfPluginZllOnOffServerLevelControlZllExtensions#
EmberAfStatus emberAfPluginZllOnOffServerLevelControlZllExtensions (uint8_t endpoint)
Level control cluster command for ZLL extensions.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | endpoint | Ver.: always |
Returns
EmberAfStatus return status