ZLL On Off Server#

Callbacks for ZLL On Off Server Component.

Callbacks#

emberAfPluginZllOnOffServerOffWithEffectCallback(uint8_t endpoint, uint8_t effectId, uint8_t effectVariant)

Off with effect.

Callbacks Documentation#

emberAfPluginZllOnOffServerOffWithEffectCallback#

EmberAfStatus emberAfPluginZllOnOffServerOffWithEffectCallback (uint8_t endpoint, uint8_t effectId, uint8_t effectVariant)

Off with effect.

Parameters
N/Aendpoint

Ver.: always

N/AeffectId

Ver.: always

N/AeffectVariant

Ver.: always

This callback is called by the ZLL On/Off Server plugin whenever an OffWithEffect command is received. The application should implement the effect and variant requested in the command and return EMBER_ZCL_STATUS_SUCCESS if successful or an appropriate error status otherwise.

Returns

  • EmberAfStatus return status


Definition at line 116 of file app/framework/plugin/zll-on-off-server/zll-on-off-server.h