GPD Address for sending and receiving a GPDF.

Public Attributes#

EmberEUI64
union EmberGpAddress::@7
uint8_t

Public Attribute Documentation#

gpdIeeeAddress#

EmberEUI64 EmberGpAddress::gpdIeeeAddress

The IEEE address is used when the application identifier is EMBER_GP_APPLICATION_IEEE_ADDRESS.


Definition at line 281 of file stack/include/gp-types.h

sourceId#

EmberGpSourceId EmberGpAddress::sourceId

The 32-bit source identifier is used when the application identifier is EMBER_GP_APPLICATION_SOURCE_ID.


Definition at line 285 of file stack/include/gp-types.h

id#

union EmberGpAddress::@7 EmberGpAddress::id

Definition at line 286 of file stack/include/gp-types.h

applicationId#

EmberGpApplicationId EmberGpAddress::applicationId

Application identifier of the GPD.


Definition at line 288 of file stack/include/gp-types.h

endpoint#

uint8_t EmberGpAddress::endpoint

Application endpoint , only used when application identifier is EMBER_GP_APPLICATION_IEEE_ADDRESS


Definition at line 292 of file stack/include/gp-types.h