Device Table#

API and Callbacks for the Device Table Component.

Simple C-based rules engine for demonstrating automatic control through a gateway.

Modules#

EmberAfPluginDeviceTableEntry

API#

void

Send a message using the device table.

void
emberAfDeviceTableSend(EmberEUI64 eui64, uint8_t endpoint)

Send a message using the device table.

void
emberAfDeviceTableCliIndexSendWithEndpoint(uint16_t index, uint8_t endpoint)

Send a CLI command based on an index and an endpoint.

void

Send an internally-generated command.

void
emberAfDeviceTableCommandSendWithEndpoint(EmberEUI64 eui64, uint8_t endpoint)

Send an internally-generated command.

void
emberAfDeviceTableCommandIndexSendWithEndpoint(uint16_t index, uint8_t endpoint)

Send an internally-generated command.

bool
emberAfDeviceTableGetEui64FromNodeId(EmberNodeId emberNodeId, EmberEUI64 eui64)

Compute the EUI64 from the node ID in the device table.

uint16_t

Compute the node ID from the device table index.

uint16_t
emberAfDeviceTableGetEndpointFromNodeIdAndEndpoint(EmberNodeId emberNodeId, uint8_t endpoint)

Find the endpoint index from node ID and endpoint number.

uint16_t
emberAfDeviceTableGetIndexFromNodeId(EmberNodeId emberNodeId)

Find the index based on the node ID.

uint16_t

Find the index based on the EUI64.

uint16_t
emberAfDeviceTableGetIndexFromEui64AndEndpoint(EmberEUI64 eui64, uint8_t endpoint)

Find the index based on the EUI64 and endpoint.

uint16_t

Find the node ID based on the EUI64.

void
emberAfPluginDeviceTableMessageSentStatus(EmberNodeId nodeId, EmberStatus status, uint16_t profileId, uint16_t clusterId)

Change the device status based on the last sent message.

void

Send a leave message to a device based on the index.

void

Inform the device table that a message was received.

void

Kick off device table route repair.

Return a pointer to the device table structure.

Return a pointer to the device table entry.

void
emberAfDeviceTableNewDeviceJoinHandler(EmberNodeId newNodeId, EmberEUI64 newNodeEui64)

Inform the device table that a new device joined.

uint32_t

Calculate time since the device heard the last message.

bool
emberAfDeviceTableMatchEui64(EmberEUI64 a, EmberEUI64 b)

Return true if the two EUI64 parameters match.

void

Clear the device table.

void

Called when a device has been removed from the device table.

void

Called when the device table has been initialized.

Enumerations#

enum
EMBER_AF_PLUGIN_DEVICE_TABLE_STATE_NULL = 0x00
EMBER_AF_PLUGIN_DEVICE_TABLE_STATE_JOINED = 0x10
EMBER_AF_PLUGIN_DEVICE_TABLE_STATE_UNRESPONSIVE = 0x11
EMBER_AF_PLUGIN_DEVICE_TABLE_STATE_LEAVE_SENT = 0x20
EMBER_AF_PLUGIN_DEVICE_TABLE_STATE_LEFT = 0x30
EMBER_AF_PLUGIN_DEVICE_TABLE_STATE_UNKNOWN = 0xff
}

Macros#

#define
EMBER_AF_PLUGIN_DEVICE_TABLE_CLUSTER_SIZE 20
#define
EMBER_AF_PLUGIN_DEVICE_TABLE_DEVICE_TABLE_SIZE 250
#define
EMBER_AF_PLUGIN_DEVICE_TABLE_NULL_NODE_ID 0xffff
#define
EMBER_AF_PLUGIN_DEVICE_TABLE_NULL_INDEX 0xffff
#define
DEVICE_ID_ON_OFF_SWITCH 0x0000
#define
DEVICE_ID_LEVEL_CONTROL_SWITCH 0x0001
#define
DEVICE_ID_ON_OFF_OUTPUT 0x0002
#define
DEVICE_ID_LEVEL_CONTROL_OUTPUT 0x0003
#define
DEVICE_ID_SCENE_SELECTOR 0x0004
#define
DEVICE_ID_CONFIG_TOOL 0x0005
#define
DEVICE_ID_REMOTE_CONTROL 0x0006
#define
DEVICE_ID_COMBINED_INTERFACE 0x0007
#define
DEVICE_ID_RANGE_EXTENDER 0x0008
#define
DEVICE_ID_MAINS_POWER_OUTLET 0x0009
#define
DEVICE_ID_DOOR_LOCK 0x000a
#define
DEVICE_ID_DOOR_LOCK_CONTROLLER 0x000b
#define
DEVICE_ID_SIMPLE_SENSOR 0x000c
#define
DEVICE_ID_CONSUMPTION_AWARENESS_DEVICE 0x000d
#define
DEVICE_ID_HOME_GATEWAY 0x0050
#define
DEVICE_ID_SMART_PLUG 0x0051
#define
DEVICE_ID_WHITE_GOODS 0x0052
#define
DEVICE_ID_METER_INTERFACE 0x0053
#define
DEVICE_ID_ON_OFF_LIGHT 0x0100
#define
DEVICE_ID_DIMMABLE_LIGHT 0x0101
#define
DEVICE_ID_COLOR_DIMMABLE_LIGHT 0x0102
#define
DEVICE_ID_ON_OFF_LIGHT_SWITCH 0x0103
#define
DEVICE_ID_DIMMER_SWITCH 0x0104
#define
DEVICE_ID_COLOR_DIMMER_SWITCH 0x0105
#define
DEVICE_ID_LIGHT_SENSOR 0x0106
#define
DEVICE_ID_OCCUPANCY_SENSOR 0x0107
#define
DEVICE_ID_SHADE 0x0200
#define
DEVICE_ID_SHADE_CONTROLLER 0x0201
#define
DEVICE_ID_WINDOW_COVERING_DEVICE 0x0202
#define
DEVICE_ID_WINDOW_COVERING_CONTROLLER 0x0203
#define
DEVICE_ID_HEATING_COOLING_UNIT 0x0300
#define
DEVICE_ID_THERMOSTAT 0x0301
#define
DEVICE_ID_TEMPERATURE_SENSOR 0x0302
#define
DEVICE_ID_PUMP 0x0303
#define
DEVICE_ID_PUMP_CONTROLLER 0x0304
#define
DEVICE_ID_PRESSURE_SENSOR 0x0305
#define
DEVICE_ID_FLOW_SENSOR 0x0306
#define
DEVICE_ID_MINI_SPLIT_AC 0x0307
#define
DEVICE_ID_IAS_CIE 0x0400
#define
DEVICE_ID_IAS_ANCILLARY_CONTROL 0x0401
#define
DEVICE_ID_IAS_ZONE 0x0402
#define
DEVICE_ID_IAS_WARNING 0x0403

API Documentation#

emberAfDeviceTableCliIndexSend#

void emberAfDeviceTableCliIndexSend (uint16_t index)

Send a message using the device table.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/Aindex

The index of the device to which to send the CLI command.

Sends the current framework ZCL command to the device specified by an index.


emberAfDeviceTableSend#

void emberAfDeviceTableSend (EmberEUI64 eui64, uint8_t endpoint)

Send a message using the device table.

Parameters
TypeDirectionArgument NameDescription
EmberEUI64N/Aeui64

EUI64 to which to send the CLI command.

uint8_tN/Aendpoint

Endpoint of the device to which to send the CLI command.

Sends the current framework ZCL command using a device specified by the EUI64 and endpoint.


emberAfDeviceTableCliIndexSendWithEndpoint#

void emberAfDeviceTableCliIndexSendWithEndpoint (uint16_t index, uint8_t endpoint)

Send a CLI command based on an index and an endpoint.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/Aindex

The index of the device to which to send the command.

uint8_tN/Aendpoint

The endpoint of the device to which to send the command.

Sends the current framework ZCL command using a device indexed in the device table.


emberAfDeviceTableCommandIndexSend#

void emberAfDeviceTableCommandIndexSend (uint16_t index)

Send an internally-generated command.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/Aindex

index of the device to which to send the command.

Sends an internally-generated command, such as generated by the emberAfFillCommandOnOffClusterOn(); command. Note: this is different from the above send command, which works with the CLI-generated outgoing commands.


emberAfDeviceTableCommandSendWithEndpoint#

void emberAfDeviceTableCommandSendWithEndpoint (EmberEUI64 eui64, uint8_t endpoint)

Send an internally-generated command.

Parameters
TypeDirectionArgument NameDescription
EmberEUI64N/Aeui64

EUI64 of the device to which to send the command.

uint8_tN/Aendpoint

The endpoint of the device to which to send the command.

Sends an internally-generated command, such as generated by the emberAfFillCommandOnOffClusterOn(); command. Note: this is different from the above send command, which works with the CLI-generated outgoing commands.


emberAfDeviceTableCommandIndexSendWithEndpoint#

void emberAfDeviceTableCommandIndexSendWithEndpoint (uint16_t index, uint8_t endpoint)

Send an internally-generated command.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/Aindex

The index of the device to which to send the command.

uint8_tN/Aendpoint

The endpoint of the device to which to send the command.

Sends an internally-generated command, such as generated by the emberAfFillCommandOnOffClusterOn(); command. Note: this is different from the above send command, which works with the CLI-generated outgoing commands.


emberAfDeviceTableGetEui64FromNodeId#

bool emberAfDeviceTableGetEui64FromNodeId (EmberNodeId emberNodeId, EmberEUI64 eui64)

Compute the EUI64 from the node ID in the device table.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AemberNodeId

The node ID of the device.

EmberEUI64N/Aeui64

The location of the EUI64 variable.

This function looks up the device-table entry using the node ID and return the EUI64.

Returns

  • bool True if an EUI can be found, false if not.


emberAfDeviceTableGetNodeIdFromIndex#

uint16_t emberAfDeviceTableGetNodeIdFromIndex (uint16_t index)

Compute the node ID from the device table index.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/Aindex

The index of the device.

Looks up the device table entry based on the index and returns the node ID.

Returns

  • The node ID of the device.


emberAfDeviceTableGetEndpointFromNodeIdAndEndpoint#

uint16_t emberAfDeviceTableGetEndpointFromNodeIdAndEndpoint (EmberNodeId emberNodeId, uint8_t endpoint)

Find the endpoint index from node ID and endpoint number.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AemberNodeId

The node ID of the device.

uint8_tN/Aendpoint

The desired endpoint.

Computes the index into the endpoint table based on the node ID and the endpoint number.

Returns

  • The index of the device.


emberAfDeviceTableGetIndexFromNodeId#

uint16_t emberAfDeviceTableGetIndexFromNodeId (EmberNodeId emberNodeId)

Find the index based on the node ID.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AemberNodeId

The node ID of the current device.

Computes the device-table index based on the node ID.

Returns

  • The index in the device-table.


emberAfDeviceTableGetFirstIndexFromEui64#

uint16_t emberAfDeviceTableGetFirstIndexFromEui64 (EmberEUI64 eui64)

Find the index based on the EUI64.

Parameters
TypeDirectionArgument NameDescription
EmberEUI64N/Aeui64

EUI64 of the desired node ID.

Computes the first device table index from the EUI64.

Returns

  • The first index that matches the EUI64.


emberAfDeviceTableGetIndexFromEui64AndEndpoint#

uint16_t emberAfDeviceTableGetIndexFromEui64AndEndpoint (EmberEUI64 eui64, uint8_t endpoint)

Find the index based on the EUI64 and endpoint.

Parameters
TypeDirectionArgument NameDescription
EmberEUI64N/Aeui64

EUI64 of the desired index.

uint8_tN/Aendpoint

The endpoint for the desired index.

Computes the node ID based on the device table entry that matches the EUI64.

Returns

  • Index that matches the EUI64


emberAfDeviceTableGetNodeIdFromEui64#

uint16_t emberAfDeviceTableGetNodeIdFromEui64 (EmberEUI64 eui64)

Find the node ID based on the EUI64.

Parameters
TypeDirectionArgument NameDescription
EmberEUI64N/Aeui64

EUI64 of the desired node ID.

Computes the node ID based on the device table entry that matches the EUI64.

Returns

  • The node ID that matches the EUI64.


emberAfPluginDeviceTableMessageSentStatus#

void emberAfPluginDeviceTableMessageSentStatus (EmberNodeId nodeId, EmberStatus status, uint16_t profileId, uint16_t clusterId)

Change the device status based on the last sent message.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AnodeId

The node ID in the last outgoing message.

EmberStatusN/Astatus

EmberStatus of the last outgoing message.

uint16_tN/AprofileId

The profile ID of the last outgoing message.

uint16_tN/AclusterId

The cluster ID of the last outgoing message.

If the last sent message was a success, change the device state to "joined". However, if the last message sent was not a success, change the device state to unresponsive.


emberAfPluginDeviceTableSendLeave#

void emberAfPluginDeviceTableSendLeave (uint16_t index)

Send a leave message to a device based on the index.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/Aindex

The index of the device to whom to send the leave message.

Sends a leave message to the device indicated by the index.


emberAfPluginDeviceTableMessageReceived#

void emberAfPluginDeviceTableMessageReceived (EmberNodeId nodeId)

Inform the device table that a message was received.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AnodeId

The node ID from which the last incoming message came.

The device table keeps track of whether a device has become unresponsive. Hearing from a known device causes the device table to transition the device state from "unresponsive" to "joined". Hearing from an unknown device causes the device table to discover the device, potentially fixing routing issues (i.e., if the node ID has changed).


emberAfPluginDeviceTableInitiateRouteRepair#

void emberAfPluginDeviceTableInitiateRouteRepair (EmberNodeId nodeId)

Kick off device table route repair.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AnodeId

The node ID of the newly unresponsive node.

A message was sent to the device and failed. Therefore, the route repair will be attempted and the node marked as unresponsive. Currently, route repair simply sends a broadcast message looking for the node ID based on the EUI64. It may be replaced with something more sophisticated in the future.


emberAfDeviceTablePointer#

EmberAfPluginDeviceTableEntry * emberAfDeviceTablePointer (void )

Return a pointer to the device table structure.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns a pointer to the device table structure.

Returns

  • A pointer to the device table structure.


emberAfDeviceTableFindDeviceTableEntry#

EmberAfPluginDeviceTableEntry * emberAfDeviceTableFindDeviceTableEntry (uint16_t index)

Return a pointer to the device table entry.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/Aindex

The index of the device table entry in which we are interested.

Returns a pointer to the device table entry based on the device table index.

Returns

  • A pointer to the device table entry.


emberAfDeviceTableNewDeviceJoinHandler#

void emberAfDeviceTableNewDeviceJoinHandler (EmberNodeId newNodeId, EmberEUI64 newNodeEui64)

Inform the device table that a new device joined.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AnewNodeId

The node ID of the newly joined device.

EmberEUI64N/AnewNodeEui64

The EUI64 of the newly joined device.

Call this function in the device table when a device joins, rejoins, or sends an end-device announce. If the device is new, it will generate a new device table entry and kick off the discovery process. If the device is not new, the device-table will make sure the node ID matches the EUI64 and make an update if necessary. It will also check to verify the discovery process has completed and attempt to complete it.


emberAfDeviceTableTimeSinceLastMessage#

uint32_t emberAfDeviceTableTimeSinceLastMessage (uint16_t index)

Calculate time since the device heard the last message.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/Aindex

The index of the device.

Computes the amount of time, in seconds, since receiving a message from the device.

Returns

  • The time since the last message (in seconds).


emberAfDeviceTableMatchEui64#

bool emberAfDeviceTableMatchEui64 (EmberEUI64 a, EmberEUI64 b)

Return true if the two EUI64 parameters match.

Parameters
TypeDirectionArgument NameDescription
EmberEUI64N/Aa

The first EUI64 to compare.

EmberEUI64N/Ab

The second EUI64 to compare.

Determines whether two EUI64 values are the same. The function will print a feedback message to indicate if both EUI64 values are NULL. The function will also print out a feedback message to indicate if the EUI64 values match but in reverse order.


emberAfDeviceTableClear#

void emberAfDeviceTableClear (void )

Clear the device table.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Clears the device table and the backup file of the device table is also cleared if it is a host.


emberAfPluginDeviceTableIndexRemovedCallback#

void emberAfPluginDeviceTableIndexRemovedCallback (uint16_t currentIndex)

Called when a device has been removed from the device table.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/AcurrentIndex

Index of the removed device.

Called when the device has been removed from the table.


emberAfPluginDeviceTableInitialized#

void emberAfPluginDeviceTableInitialized (void )

Called when the device table has been initialized.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Called when the device table has been initialized


Enumeration Documentation#

EmberAfPluginDeviceTableDeviceState#

EmberAfPluginDeviceTableDeviceState
Enumerator
EMBER_AF_PLUGIN_DEVICE_TABLE_STATE_NULL
EMBER_AF_PLUGIN_DEVICE_TABLE_STATE_JOINED
EMBER_AF_PLUGIN_DEVICE_TABLE_STATE_UNRESPONSIVE
EMBER_AF_PLUGIN_DEVICE_TABLE_STATE_LEAVE_SENT
EMBER_AF_PLUGIN_DEVICE_TABLE_STATE_LEFT
EMBER_AF_PLUGIN_DEVICE_TABLE_STATE_UNKNOWN

Typedef Documentation#

EmberAfPluginDeviceTableDeviceState#

typedef uint8_t EmberAfPluginDeviceTableDeviceState