End Device Support#

API and Callbacks for the End Device Support Component.

Silicon Labs implementation of polling for end devices. Note that the Poll Control Server component sets the long and short poll intervals at startup. If both components are enabled, the long and short poll intervals set here will not be used.

Modules#

End Device Support

Handlers#

Handlers Documentation#

emberAfPluginEndDeviceSupportMoveNetworkEventHandler#

void emberAfPluginEndDeviceSupportMoveNetworkEventHandler (sl_zigbee_event_t * event)
Parameters
TypeDirectionArgument NameDescription
sl_zigbee_event_t *N/Aevent

Definition at line 70 of file app/framework/plugin/end-device-support/end-device-support.h