OTA Client#
API and Callbacks for the OTA Cluster Client Component.
Silicon Labs implementation of the Zigbee Over-the-air Bootload Client Cluster (a multi-hop, application bootloader). This implementation finds the OTA server in the network, periodically queries the server for a new image to download, downloads the data, and then waits for the server command to tell it to upgrade. Optionally, it can cryptographically verify the image before upgrade.
Modules#
API#
Set whether OTA clients use non TC servers.
Set whether OTA clients use non TC servers.
Return the current value of ignoreNonTrustCenter for OTA clients.
Set whether OTA Clients will permit firmware downgrades.
Return the current value of disableOtaDowngrades.
Variables#
Macros#
API Documentation#
emberAfOtaServerSendUpgradeRequest#
void emberAfOtaServerSendUpgradeRequest ( IgnoreNonTc)
Set whether OTA clients use non TC servers.
Type | Direction | Argument Name | Description |
---|---|---|---|
N/A | IgnoreNonTc | a bool determining whether client should ignore any non Trust Center OTA servers |
Sets the behavior of OTA clients when determining whether or not to use non Trust Center OTA servers and abort any download that is in progress.
emberAfPluginOtaClientSetIgnoreNonTrustCenter#
void emberAfPluginOtaClientSetIgnoreNonTrustCenter (bool ignoreNonTc)
Set whether OTA clients use non TC servers.
Type | Direction | Argument Name | Description |
---|---|---|---|
bool | N/A | ignoreNonTc | a bool determining whether client should ignore any non Trust Center OTA servers |
Sets the behavior of OTA clients when determining whether or not to use non Trust Center OTA servers and abort any download that is in progress.
emberAfPluginOtaClientGetIgnoreNonTrustCenter#
bool emberAfPluginOtaClientGetIgnoreNonTrustCenter ()
Return the current value of ignoreNonTrustCenter for OTA clients.
emberAfPluginSetDisableOtaDowngrades#
void emberAfPluginSetDisableOtaDowngrades (bool isDisabled)
Set whether OTA Clients will permit firmware downgrades.
Type | Direction | Argument Name | Description |
---|---|---|---|
bool | N/A | isDisabled | A bool value indicating whether or not downgrades will be disabled |
emberAfPluginGetDisableOtaDowngrades#
bool emberAfPluginGetDisableOtaDowngrades ()
Return the current value of disableOtaDowngrades.
Variable Documentation#
sli_zigbee_af_ota_client_stopDownloadPercentage#
uint8_t sli_zigbee_af_ota_client_stopDownloadPercentage