ZLL Commissioning Client#

API and Callbacks for the ZLL Commissioning Cluster Client Component.

Client side implementation of the ZigBee 3.0 touchlink commissioning mechanism.

Modules#

ZLL Commissioning

API#

EmberStatus

Initiate the touch link procedure.

EmberStatus

Initiate a touch link to retrieve information about a target device.

EmberStatus

Initiate a touch link to cause a target device to identify itself.

EmberStatus

Initiate a touch link for the purpose of resetting a target device.

void

Abort the touch link procedure.

API Documentation#

emberAfZllInitiateTouchLink#

EmberStatus emberAfZllInitiateTouchLink (void )

Initiate the touch link procedure.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function causes the stack to broadcast a series of ScanRequest commands via inter-PAN messaging. The plugin selects the target that sent a ScanResponse command with the strongest RSSI and attempts to link with it. If touch linking completes successfully, the plugin calls emberAfPluginZllCommissioningTouchLinkCompleteCallback with information about the network and the target. If touch linking fails, the plugin calls emberAfPluginZllCommissioningTouchLinkFailedCallback.

Returns

  • An ::EmberStatus value that indicates the success or failure of the command.


emberAfZllDeviceInformationRequest#

EmberStatus emberAfZllDeviceInformationRequest (void )

Initiate a touch link to retrieve information about a target device.

Parameters
TypeDirectionArgument NameDescription
voidN/A

As with a traditional touch link, this function causes the stack to broadcast messages to discover a target device. When the target is selected (based on RSSI), the plugin will retrieve information about it by unicasting a series of DeviceInformationRequest commands via inter-PAN messaging. If the process completes successfully, the plugin calls emberAfPluginZllCommissioningTouchLinkCompleteCallback with information about the target. If touch linking fails, the plugin calls emberAfPluginZllCommissioningTouchLinkFailedCallback.

Returns

  • An ::EmberStatus value that indicates the success or failure of the command.


emberAfZllIdentifyRequest#

EmberStatus emberAfZllIdentifyRequest (void )

Initiate a touch link to cause a target device to identify itself.

Parameters
TypeDirectionArgument NameDescription
voidN/A

As with a traditional touch link, this function causes the stack to broadcast messages to discover a target device. When the target is selected (based on RSSI), the plugin will cause it to identify itself by unicasting an IdentifyRequest command via inter-PAN messaging. If the process completes successfully, the plugin calls emberAfPluginZllCommissioningTouchLinkCompleteCallback with information about the target. If touch linking fails, the plugin calls emberAfPluginZllCommissioningTouchLinkFailedCallback.

Returns

  • An ::EmberStatus value that indicates the success or failure of the command.


emberAfZllResetToFactoryNewRequest#

EmberStatus emberAfZllResetToFactoryNewRequest (void )

Initiate a touch link for the purpose of resetting a target device.

Parameters
TypeDirectionArgument NameDescription
voidN/A

As with a traditional touch link, this function causes the stack to broadcast messages to discover a target device. When the target is selected (based on RSSI), the plugin will reset it by unicasting a ResetToFactoryNewRequest command via inter-PAN messaging. If the process completes successfully, the plugin calls emberAfPluginZllCommissioningTouchLinkCompleteCallback with information about the target. If touch linking fails, the plugin calls emberAfPluginZllCommissioningTouchLinkFailedCallback.

Returns

  • An ::EmberStatus value that indicates the success or failure of the command.


emberAfZllAbortTouchLink#

void emberAfZllAbortTouchLink (void )

Abort the touch link procedure.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function can be called to cancel the touch link procedure. This can be useful, for example, if the touch link target is incorrect.