Cluster Commands: Scenes#
This group describes the CLI commands for the Scenes cluster. Listed below is a description of the cluster:
Attributes and commands for scene configuration and manipulation.
Macros#
zcl scenes add [groupId:2] [sceneId:1] [transitionTime:2] [sceneName:-1] [extensionFieldSets:4]
zcl scenes view [groupId:2] [sceneId:1]
zcl scenes remove [groupId:2] [sceneId:1]
zcl scenes rmall [groupId:2]
zcl scenes store [groupId:2] [sceneId:1]
zcl scenes recall [groupId:2] [sceneId:1] [transitionTime:2]
zcl scenes get [groupId:2]
zcl scenes eadd [groupId:2] [sceneId:1] [transitionTime:2] [sceneName:-1] [extensionFieldSets:4]
zcl scenes eview [groupId:2] [sceneId:1]
zcl scenes copy [mode:1] [groupIdFrom:2] [sceneIdFrom:1] [groupIdTo:2] [sceneIdTo:1]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_ADD#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_ADD
zcl scenes add [groupId:2] [sceneId:1] [transitionTime:2] [sceneName:-1] [extensionFieldSets:4]
Add a scene to the scene table. Extension field sets are supported, and are inputed as arrays of the form [[cluster ID] [length] [value0...n] ...]
groupId - INT16U
sceneId - INT8U
transitionTime - INT16U
sceneName - CHAR_STRING
extensionFieldSets - struct SceneExtensionFieldSet
EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_VIEW#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_VIEW
zcl scenes view [groupId:2] [sceneId:1]
Command description for ViewScene
groupId - INT16U
sceneId - INT8U
EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_REMOVE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_REMOVE
zcl scenes remove [groupId:2] [sceneId:1]
Command description for RemoveScene
groupId - INT16U
sceneId - INT8U
EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_RMALL#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_RMALL
zcl scenes rmall [groupId:2]
Command description for RemoveAllScenes
groupId - INT16U
EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_STORE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_STORE
zcl scenes store [groupId:2] [sceneId:1]
Command description for StoreScene
groupId - INT16U
sceneId - INT8U
EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_RECALL#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_RECALL
zcl scenes recall [groupId:2] [sceneId:1] [transitionTime:2]
Command description for RecallScene
groupId - INT16U
sceneId - INT8U
transitionTime - INT16U
EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_GET#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_GET
zcl scenes get [groupId:2]
Command description for GetSceneMembership
groupId - INT16U
EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_EADD#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_EADD
zcl scenes eadd [groupId:2] [sceneId:1] [transitionTime:2] [sceneName:-1] [extensionFieldSets:4]
Command description for EnhancedAddScene
groupId - INT16U
sceneId - INT8U
transitionTime - INT16U
sceneName - CHAR_STRING
extensionFieldSets - struct SceneExtensionFieldSet
EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_EVIEW#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_EVIEW
zcl scenes eview [groupId:2] [sceneId:1]
Command description for EnhancedViewScene
groupId - INT16U
sceneId - INT8U
EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_COPY#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_COPY
zcl scenes copy [mode:1] [groupIdFrom:2] [sceneIdFrom:1] [groupIdTo:2] [sceneIdTo:1]
Command description for CopyScene
mode - ScenesCopyMode [BITMAP8]
groupIdFrom - INT16U
sceneIdFrom - INT8U
groupIdTo - INT16U
sceneIdTo - INT8U