You are viewing documentation for version:7.5.1GP Tx queue entry. Public Attributes#boolinUsebooluseCcaEmberGpAddressaddruint8_tgpdCommandIdEmberMessageBufferasduuint8_tgpepHandleuint16_tqueueEntryLifetimeMsPublic Attribute Documentation#inUse#bool EmberGpTxQueueEntry::inUseThe entry in use useCca#bool EmberGpTxQueueEntry::useCcaUse CCA during transmit addr#EmberGpAddress EmberGpTxQueueEntry::addrGP address gpdCommandId#uint8_t EmberGpTxQueueEntry::gpdCommandIdGPD Command ID asdu#EmberMessageBuffer EmberGpTxQueueEntry::asduBuffer holding ASDU gpepHandle#uint8_t EmberGpTxQueueEntry::gpepHandleHandle for the outgoing message queueEntryLifetimeMs#uint16_t EmberGpTxQueueEntry::queueEntryLifetimeMsLife time in milliseconds for the entry to expire, 0 indicates no expiry