Cluster Commands: Device Management#
This group describes the CLI commands for the Device Management cluster. Listed below is a description of the cluster: This cluster provides attributes and commands to support device-cognisant application layer protocols.
Macros#
zcl dm get-chg-of-tenancy
zcl dm get-chg-of-supplier
zcl dm req-new-pass [passwordType:1]
zcl dm get-site-id
zcl dm rpt-event-config [commandIndex:1] [totalCommands:1] [eventConfigurationPayload:3]
zcl dm get-cin
zcl dm pub-chg-of-supplier [currentProviderId:4] [issuerEventId:4] [tariffType:1] [proposedProviderId:4] [providerChangeImplementationTime:4] [providerChangeControl:4] [proposedProviderName:-1] [proposedProviderContactDetails:-1]
zcl dm req-new-pass-resp [issuerEventId:4] [implementationDateTime:4] [durationInMinutes:2] [passwordType:1] [password:-1]
zcl dm set-event-config [issuerEventId:4] [startDateTime:4] [eventConfiguration:1] [configurationControl:1] [eventConfigurationPayload:1]
zcl dm get-event-config [eventId:2]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_CHG_OF_TENANCY#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_CHG_OF_TENANCY
zcl dm get-chg-of-tenancy
This command is used to request the ESI to respond with information regarding any available change of tenancy.
EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_CHG_OF_SUPPLIER#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_CHG_OF_SUPPLIER
zcl dm get-chg-of-supplier
This command is used to request the ESI to respond with information regarding any available change of supplier.
EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_REQ_NEW_PASS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_REQ_NEW_PASS
zcl dm req-new-pass [passwordType:1]
This command is used to request the current password from the server.
passwordType - PasswordType [ENUM8] See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_SITE_ID#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_SITE_ID
zcl dm get-site-id
This command is used to request the ESI to respond with information regarding any pending change of Site ID.
EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_RPT_EVENT_CONFIG#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_RPT_EVENT_CONFIG
zcl dm rpt-event-config [commandIndex:1] [totalCommands:1] [eventConfigurationPayload:3]
This command is sent in response to a GetEventConfiguration command.
commandIndex - INT8U
totalCommands - INT8U
eventConfigurationPayload - struct sl_zigbee_zcl_event_configuration_payload_t
EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_CIN#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_CIN
zcl dm get-cin
This command is used to request the ESI to respond with information regarding any pending change of Customer ID Number.
EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_PUB_CHG_OF_SUPPLIER#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_PUB_CHG_OF_SUPPLIER
zcl dm pub-chg-of-supplier [currentProviderId:4] [issuerEventId:4] [tariffType:1] [proposedProviderId:4] [providerChangeImplementationTime:4] [providerChangeControl:4] [proposedProviderName:-1] [proposedProviderContactDetails:-1]
This command is used to change the Supplier (energy supplier) that is supplying the meter (s).
currentProviderId - INT32U
issuerEventId - INT32U
tariffType - TariffType [ENUM8]
proposedProviderId - INT32U
providerChangeImplementationTime - UTC_TIME
providerChangeControl - ProposedChangeControl [BITMAP32]
proposedProviderName - OCTET_STRING
proposedProviderContactDetails - OCTET_STRING See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_REQ_NEW_PASS_RESP#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_REQ_NEW_PASS_RESP
zcl dm req-new-pass-resp [issuerEventId:4] [implementationDateTime:4] [durationInMinutes:2] [passwordType:1] [password:-1]
This command is used to send the current password to the client.
issuerEventId - INT32U
implementationDateTime - UTC_TIME
durationInMinutes - INT16U
passwordType - PasswordType [ENUM8]
password - OCTET_STRING See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_SET_EVENT_CONFIG#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_SET_EVENT_CONFIG
zcl dm set-event-config [issuerEventId:4] [startDateTime:4] [eventConfiguration:1] [configurationControl:1] [eventConfigurationPayload:1]
This command provides a method to set the event configuration attributes, held in a client device.
issuerEventId - INT32U
startDateTime - UTC_TIME
eventConfiguration - EventConfiguration [BITMAP8]
configurationControl - EventConfigurationControl [ENUM8]
eventConfigurationPayload - INT8U See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_EVENT_CONFIG#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_EVENT_CONFIG
zcl dm get-event-config [eventId:2]
This command allows the server to request details of event configurations.
eventId - INT16U