Level Control Server#
API and Callbacks for the Level Control Cluster Server Component.
Silicon Labs implementation of the Level Control server cluster. If the ZLL Level Control server cluster component is also enabled, this component uses it to handle ZLL enhancements. Otherwise, all ZLL extensions are disabled. It is not intended for production but provides sample code to show how the cluster could be implemented.
This group describes the CLI commands for the Level Control cluster. Listed below is a description of the cluster: Attributes and commands for controlling devices that can be set to a level between fully 'On' and fully 'Off.'
Modules#
Macros#
zcl level-control mv-to-level [level:1] [transitionTime:2] [optionMask:1] [optionOverride:1]
zcl level-control move [moveMode:1] [rate:1] [optionMask:1] [optionOverride:1]
zcl level-control step [stepMode:1] [stepSize:1] [transitionTime:2] [optionMask:1] [optionOverride:1]
zcl level-control stop [optionMask:1] [optionOverride:1]
zcl level-control o-mv-to-level [level:1] [transitionTime:2]
zcl level-control o-move [moveMode:1] [rate:1]
zcl level-control o-step [stepMode:1] [stepSize:1] [transitionTime:2]
zcl level-control o-stop
zcl level-control mv-to-closest-freq [frequency:2]
Macro Definition Documentation#
SL_ZIGBEE_AF_PLUGIN_LEVEL_CONTROL_TICKS_PER_SECOND#
#define SL_ZIGBEE_AF_PLUGIN_LEVEL_CONTROL_TICKS_PER_SECONDValue:
32
SL_ZIGBEE_AF_PLUGIN_LEVEL_CONTROL_TICK_TIME#
#define SL_ZIGBEE_AF_PLUGIN_LEVEL_CONTROL_TICK_TIMEValue:
(MILLISECOND_TICKS_PER_SECOND / SL_ZIGBEE_AF_PLUGIN_LEVEL_CONTROL_TICKS_PER_SECOND)
EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MV_TO_LEVEL#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MV_TO_LEVEL
zcl level-control mv-to-level [level:1] [transitionTime:2] [optionMask:1] [optionOverride:1]
Command description for MoveToLevel
level - INT8U
transitionTime - INT16U
optionMask - BITMAP8
optionOverride - BITMAP8
EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MOVE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MOVE
zcl level-control move [moveMode:1] [rate:1] [optionMask:1] [optionOverride:1]
Command description for Move
moveMode - MoveMode [ENUM8]
rate - INT8U
optionMask - BITMAP8
optionOverride - BITMAP8 See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_STEP#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_STEP
zcl level-control step [stepMode:1] [stepSize:1] [transitionTime:2] [optionMask:1] [optionOverride:1]
Command description for Step
stepMode - StepMode [ENUM8]
stepSize - INT8U
transitionTime - INT16U
optionMask - BITMAP8
optionOverride - BITMAP8 See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_STOP#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_STOP
zcl level-control stop [optionMask:1] [optionOverride:1]
Command description for Stop
optionMask - BITMAP8
optionOverride - BITMAP8
EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_MV_TO_LEVEL#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_MV_TO_LEVEL
zcl level-control o-mv-to-level [level:1] [transitionTime:2]
Command description for MoveToLevelWithOnOff
level - INT8U
transitionTime - INT16U
EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_MOVE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_MOVE
zcl level-control o-move [moveMode:1] [rate:1]
Command description for MoveWithOnOff
moveMode - MoveMode [ENUM8]
rate - INT8U See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_STEP#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_STEP
zcl level-control o-step [stepMode:1] [stepSize:1] [transitionTime:2]
Command description for StepWithOnOff
stepMode - StepMode [ENUM8]
stepSize - INT8U
transitionTime - INT16U See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_STOP#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_STOP
zcl level-control o-stop
Command description for StopWithOnOff
EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MV_TO_CLOSEST_FREQ#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MV_TO_CLOSEST_FREQ
zcl level-control mv-to-closest-freq [frequency:2]
Command description for MoveToClosestFrequency
frequency - INT16U