ZLL Commissioning Common#
API and Callbacks for the ZLL Commissioning Common Component.
Common code for the ZigBee 3.0 touchlink commissioning mechanism. This component is required for both server and client side implementations.
Modules#
API#
Generate a random network key and initializes the security state of the device.
Indicate whether a touch link procedure is currently in progress.
Reset the local device to a factory new state.
Disable touchlink processing.
Enable touchlink processing.
Enumerations#
Macros#
API Documentation#
sl_zigbee_af_zll_set_initial_security_state#
sl_status_t sl_zigbee_af_zll_set_initial_security_state (void )
Generate a random network key and initializes the security state of the device.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function is a convenience wrapper for ::sl_zigbee_zll_set_initial_security_state, which must be called before starting or joining a network. The plugin initializes the security state for the initiator during touch linking. The target must initialize its own security state prior to forming a network either by using this function or by calling ::sl_zigbee_zll_set_initial_security_state directly.
Returns
An sl_status_t value that indicates the success or failure of the command.
sl_zigbee_af_zll_touch_link_in_progress#
bool sl_zigbee_af_zll_touch_link_in_progress (void )
Indicate whether a touch link procedure is currently in progress.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
True if a touch link is in progress or false otherwise.
sl_zigbee_af_zll_reset_to_factory_new#
void sl_zigbee_af_zll_reset_to_factory_new (void )
Reset the local device to a factory new state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function causes the device to leave the network and clear its network parameters, resets its attributes to their default values, and clears the group and scene tables.
sl_zigbee_af_zll_disable#
sl_status_t sl_zigbee_af_zll_disable (void )
Disable touchlink processing.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function will cause the device to refuse network start/join requests if it receives them and will not allow touchlinking. Note that this will have the effect of overriding the sl_zigbee_af_zll_no_touchlink_for_nfn function.
sl_zigbee_af_zll_enable#
sl_status_t sl_zigbee_af_zll_enable (void )
Enable touchlink processing.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function will cause the device to accept network start/join requests if it receives them and will not allow touchlinking. Note that this will have the effect of overriding the sl_zigbee_af_zll_no_touchlink_for_nfn function.
Enumeration Documentation#
StateEnum#
StateEnum
| Enumerator | |
|---|---|
| INITIAL | |
| SCAN_FOR_TOUCH_LINK | |
| SCAN_FOR_DEVICE_INFORMATION | |
| SCAN_FOR_IDENTIFY | |
| SCAN_FOR_RESET | |
| TARGET_NETWORK_FOUND | |
| ABORTING_TOUCH_LINK | |
| SCAN_COMPLETE | |
| TOUCH_LINK_TARGET | |
| FORMING_NETWORK | |
| RESETTING_TO_FACTORY_NEW | |
Variable Documentation#
Macro Definition Documentation#
touchLinkInProgress#
#define touchLinkInProgressValue:
sl_zigbee_af_zll_commissioning_initial_security_state_cb#
#define sl_zigbee_af_zll_commissioning_initial_security_state_cbValue:
sl_zigbee_af_zll_commissioning_common_initial_security_state_cb
sl_zigbee_af_zll_commissioning_touch_link_complete_cb#
#define sl_zigbee_af_zll_commissioning_touch_link_complete_cbValue:
sl_zigbee_af_zll_commissioning_common_touch_link_complete_cb
sl_zigbee_af_zll_commissioning_reset_to_factory_new_cb#
#define sl_zigbee_af_zll_commissioning_reset_to_factory_new_cbValue:
sl_zigbee_af_zll_commissioning_common_reset_to_factory_new_cb