Debugging Utilities#

EmberZNet debugging utilities.

See sl_zigbee_debug.h for source code.

Functions#

void
sl_zigbee_debug_assert(const char *filename, int linenumber)

Print the filename and line number to the debug serial port.

void
sl_zigbee_debug_memory_dump(uint8_t *start, uint8_t *end)

Print the contents of RAM to the debug serial port.

void
sl_zigbee_debug_binary_printf(const char *formatString,...)

Print binary data to the debug channel.

void
sli_util_debug_send_vuart_message(uint8_t *buff, uint8_t len)

Send VUART data out the debug channel.

void
sl_zigbee_debug_error(sl_status_t code)

Print an ::sl_status_t return code to the serial port.

bool

Turn off all debug output.

void

Restore the state of the debug output.

void
sl_zigbee_debug_printf(const char *formatString,...)

Prints text debug messages.

Macros#

#define

This function is obsolete and no longer required to initialize the debug system.

Function Documentation#

sl_zigbee_debug_assert#

void sl_zigbee_debug_assert (const char * filename, int linenumber)

Print the filename and line number to the debug serial port.

Parameters
TypeDirectionArgument NameDescription
const char *N/Afilename

The name of the file where the assert occurred.

intN/Alinenumber

The line number in the file where the assert occurred.


sl_zigbee_debug_memory_dump#

void sl_zigbee_debug_memory_dump (uint8_t * start, uint8_t * end)

Print the contents of RAM to the debug serial port.

Parameters
TypeDirectionArgument NameDescription
uint8_t *N/Astart

The start address of the block of RAM to dump.

uint8_t *N/Aend

The end address of the block of RAM to dump (address of the last byte).


sl_zigbee_debug_binary_printf#

void sl_zigbee_debug_binary_printf (const char * formatString, ... )

Print binary data to the debug channel.

Parameters
TypeDirectionArgument NameDescription
const char *N/AformatString

A string of conversion specification characters describing the arguments to be printed.

...N/A

The arguments to be printed.

This function does not use the normal printf format conventions. To print text debug messages, use sl_zigbee_debug_printf(). The format string must contain only these conversion specification characters:

  • B - uint8_t value.

  • W - uint16_t value, printed least significant byte first.

  • D - uint32_t value, printed least significant byte first.

  • F - pointer to null terminated string in Flash (const char *).

  • xxxp - pointer to RAM, length is xxx (max 255).

  • lp - pointer to RAM, length is uint8_t argument.

  • xxxf - pointer to Flash (const char *), length is xxx (max 255).

  • lf - pointer to Flash (const char *), length is uint8_t argument.

  • b - sli_buffer_manager_buffer_t.

Examples:

sl_zigbee_debug_binary_printf("BWD", status, panId, channelMask);
sl_zigbee_debug_binary_printf("F8p", "string example", eui64);
sl_zigbee_debug_binary_printf("lp64fb", length, bytes, dataTable, buffer);

sli_util_debug_send_vuart_message#

void sli_util_debug_send_vuart_message (uint8_t * buff, uint8_t len)

Send VUART data out the debug channel.

Parameters
TypeDirectionArgument NameDescription
uint8_t *N/Abuff

A pointer to the data to send.

uint8_tN/Alen

The length of the data to send.


sl_zigbee_debug_error#

void sl_zigbee_debug_error (sl_status_t code)

Print an ::sl_status_t return code to the serial port.

Parameters
TypeDirectionArgument NameDescription
sl_status_tN/Acode

The ::sl_status_t code to print.


sl_zigbee_debug_report_off#

bool sl_zigbee_debug_report_off (void )

Turn off all debug output.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • The current state (true for on, false for off).


sl_zigbee_debug_report_restore#

void sl_zigbee_debug_report_restore (bool state)

Restore the state of the debug output.

Parameters
TypeDirectionArgument NameDescription
boolN/Astate

The state returned from sl_zigbee_debug_report_off(). This is done so that debug output is not blindly turned on.


sl_zigbee_debug_printf#

void sl_zigbee_debug_printf (const char * formatString, ... )

Prints text debug messages.

Parameters
TypeDirectionArgument NameDescription
const char *N/AformatString

Takes the following:

...N/A

%%

Percent sign

%c

Single-byte char

%s

RAM string

%p

Flash string (does not follow the printf standard)

%u

Two-byte unsigned decimal

%d

Two-byte signed decimal

%x, %%2x, %%4x

1-, 2-, 4-byte hex value (always 0 padded; does not follow the printf standard)


Macro Definition Documentation#

sl_zigbee_debug_init#

#define sl_zigbee_debug_init
Value:
(port)

This function is obsolete and no longer required to initialize the debug system.


DEBUG_ROUTINES_PRESENT#

#define DEBUG_ROUTINES_PRESENT