Multi-Network Manager#
SL_ZIGBEE_MULTI_NETWORK_STRIPPED is an optional #define that is used on flash-space constrained chips to conditionally compile out multi-network related source code.
Functions#
uint8_t
Return the current network index.
sl_status_t
sl_zigbee_set_current_network(uint8_t index)
Set the current network.
uint8_t
Can only be called inside an application callback.
Function Documentation#
sl_zigbee_get_current_network#
uint8_t sl_zigbee_get_current_network (void )
Return the current network index.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
sl_zigbee_set_current_network#
sl_status_t sl_zigbee_set_current_network (uint8_t index)
Set the current network.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | index | The network index. |
Returns
::SL_STATUS_INVALID_INDEX if the index does not correspond to a valid network, and ::SL_STATUS_OK otherwise.
sl_zigbee_get_callback_network#
uint8_t sl_zigbee_get_callback_network (void )
Can only be called inside an application callback.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
the index of the network the callback refers to. If this function is called outside of a callback, it returns 0xFF.