Device Control#
API for the Device Control functionality in the Application Framework.
Device Control description.
API#
bool
sl_zigbee_af_is_device_enabled(uint8_t endpoint)
Check whether the endpoint is enabled.
bool
sl_zigbee_af_is_device_identifying(uint8_t endpoint)
Check whether the endpoint is identifying.
void
sl_zigbee_af_set_device_enabled(uint8_t endpoint, bool enabled)
Enable or disable an endpoint.
API Documentation#
sl_zigbee_af_is_device_enabled#
bool sl_zigbee_af_is_device_enabled (uint8_t endpoint)
Check whether the endpoint is enabled.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | endpoint | Zigbee endpoint number |
This function returns true if device at a given endpoint is enabled. At startup, all endpoints are enabled.
sl_zigbee_af_is_device_identifying#
bool sl_zigbee_af_is_device_identifying (uint8_t endpoint)
Check whether the endpoint is identifying.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | endpoint | Zigbee endpoint number |
This function returns true if the device at a given endpoint is identifying.
sl_zigbee_af_set_device_enabled#
void sl_zigbee_af_set_device_enabled (uint8_t endpoint, bool enabled)
Enable or disable an endpoint.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | endpoint | Zigbee endpoint number |
| bool | N/A | enabled |
By calling this function, you turn off all processing of incoming traffic for a given endpoint.