Security and Crypto#
The Security and Crypto module provides interfaces for implementing cryptographic operations within the Sidewalk SDK. These interfaces ensure secure data transmission and storage by offering functionalities such as encryption, decryption, hashing, and key management, enabling developers to protect sensitive information across different hardware platforms.
Modules#
Functions#
Initialize sid_pal crypto HAL.
Deinitialize crypto HAL.
Generate random number.
Generate hash.
Generate HMAC.
Encrypt or decrypt using following AES algorithm.
Encrypt or decrypt using AEAD algorithm.
Sign or verify elliptic curve digital signature using given algorithm.
Generate shared secret using private key and public key.
Generate ECC key pair using given algorithm.
Function Documentation#
sid_pal_crypto_init#
sid_error_t sid_pal_crypto_init (void )
Initialize sid_pal crypto HAL.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
This function initializes the SID PAL crypto HAL and prepares it for cryptographic operations.
sid_pal_crypto_deinit#
sid_error_t sid_pal_crypto_deinit (void )
Deinitialize crypto HAL.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
This function deinitializes the SID PAL crypto HAL and releases any resources that were allocated.
sid_pal_crypto_rand#
sid_error_t sid_pal_crypto_rand (uint8_t * rand, size_t size)
Generate random number.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t * | [out] | rand | Pointer to rand buffer.  | 
| size_t | [in] | size | Size of rand number  | 
This function generates a random number and stores it in the provided buffer.
sid_pal_crypto_hash#
sid_error_t sid_pal_crypto_hash (sid_pal_hash_params_t * params)
Generate hash.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sid_pal_hash_params_t * | [inout] | params | Pointer to the hash parameters.  | 
SHA256 and SHA512 is now supported.
This function generates a hash using the specified parameters.
sid_pal_crypto_hmac#
sid_error_t sid_pal_crypto_hmac (sid_pal_hmac_params_t * params)
Generate HMAC.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sid_pal_hmac_params_t * | [inout] | params | Pointer to the hash parameters.  | 
HMAC/SHA256 and HMAC/SHA512 is now supported.
This function generates an HMAC using the specified parameters.
sid_pal_crypto_aes_crypt#
sid_error_t sid_pal_crypto_aes_crypt (sid_pal_aes_params_t * params)
Encrypt or decrypt using following AES algorithm.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sid_pal_aes_params_t * | [inout] | params | Pointer to AES parameters.  | 
AES-CMAC AES-CTR are supported.
This function encrypts or decrypts data using the specified AES algorithm.
sid_pal_crypto_aead_crypt#
sid_error_t sid_pal_crypto_aead_crypt (sid_pal_aead_params_t * params)
Encrypt or decrypt using AEAD algorithm.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sid_pal_aead_params_t * | [inout] | params | Pointer to the AEAD parameters.  | 
This function encrypts or decrypts data using the specified AEAD algorithm.
sid_pal_crypto_ecc_dsa#
sid_error_t sid_pal_crypto_ecc_dsa (sid_pal_dsa_params_t * params)
Sign or verify elliptic curve digital signature using given algorithm.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sid_pal_dsa_params_t * | [inout] | params | Pointer to the ECC DSA parameters.  | 
This function signs or verifies an elliptic curve digital signature using the specified parameters.
sid_pal_crypto_ecc_ecdh#
sid_error_t sid_pal_crypto_ecc_ecdh (sid_pal_ecdh_params_t * params)
Generate shared secret using private key and public key.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sid_pal_ecdh_params_t * | [inout] | params | Pointer to the ECDH parameters.  | 
This function generates a shared secret using the specified private key and public key.
sid_pal_crypto_ecc_key_gen#
sid_error_t sid_pal_crypto_ecc_key_gen (sid_pal_ecc_key_gen_params_t * params)
Generate ECC key pair using given algorithm.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sid_pal_ecc_key_gen_params_t * | [inout] | params | Generate ECC key pair using given algorithm.  | 
This function generates an ECC key pair using the specified algorithm.