Edit

Amazon Sidewalk - SoC Bluetooth Sub-GHz CLI Application#

The Bluetooth sub-GHz Command Line Interface (CLI) sample application allows the user to interact with the endpoint using CLI commands. The application leverages the Amazon Sidewalk protocol to exchange data between the endpoint and the AWS Cloud using one of the 3 radio layers. It is possible to initialize and start the stack using any one of the 3 radio layers (BLE, FSK, or CSS). A one-time registration phase (using either BLE or FSK, as registration does not occur over CSS) is required at first boot.

Ⓘ INFO Ⓘ: This application can be used with the KG100S module or Sidewalk-supported EFR32 series 2 SoCs with at least 768kB flash size.

⚠ WARNING ⚠: Sub-GHz communication (FSK and CSS) occurs in the 900MHz band, a frequency open in the US but may be restricted in other regions.

Prerequisites#

To successfully interface with Amazon Sidewalk, this example application requires the preparation of cloud (AWS) resources and the addition of device credentials matched to those resources. In order to perform these tasks and procure access to a Sidewalk gateway, complete the initial software and hardware setup steps described in Getting Started: Prerequisites.

Ⓘ INFO Ⓘ: Make note of the additional sub-GHz considerations discussed in the Silicon Labs Wireless Development Kit section of the hardware prequisites.

Build the Application#

With prerequisites in place, generate the primary application image as described in Getting Started: Create and Compile your Sidewalk Application.

Prepare the Cloud and Endpoint#

Create AWS resources to interface with your endpoint and couple the application image with device-specific credentials by following the steps in Getting Started: Provision your Amazon Sidewalk Device.

Interacting with the Endpoint through the CLI#

Control the endpoint's behavior and configuration using the CLI commands described in the following sections. The J-Link RTT interface provides access to the CLI commands.

Ⓘ INFO Ⓘ: When running this application for the first time on a new device, the endpoint will automatically perform a one-time Touchless Registration with Amazon Sidewalk. This only occurs over BLE or FSK (not CSS), so at first boot you must start one of these two communication links to initiate registration. Registration is a persistent state, so from that point forward any of the 3 links can be selected at will.

The CLI is divided into two sets of commands:

  • Commands starting with sidewalk or sid are used to control the Sidewalk stack.

  • Commands starting with attributes or att are used to control the stack settings.

You can display the available commands by entering help in the console.

Sidewalk Commands#

To see the available commands, enter the following command in the console:

sid help

The list of available commands is output on the console with the associated help. Following is an extended description of and examples of how to use each command.

Command

Description

Example

sid init <link(s)>

Initialize Sidewalk stack for the selected communication link or links (ble/fsk/css). This function can only be called once. You have to use deinit to call it again.

> sid init ble+fsk

sid start <link(s)>

Start Sidewalk stack for the selected communication link (ble/fsk/css).

> sid start ble+fsk+css

sid stop <link(s)>

Stop Sidewalk stack for the selected communication link (ble/fsk/css).

> sid stop ble+fsk

sid deinit

Deinitialize Sidewalk stack.

> sid deinit

sid reset

Deregisters the Sidewalk device and restores settings to factory defaults.

> sid reset

sid bleconnect

Initiate BLE connection request.

> sid bleconnect

sid send <message_type> <payload> [<link(s)>]

Send a custom message to the cloud (Message types get/set/notify/response). Link (ble/fsk/css) is only for auto connect mode.

> sid send notify ascii_encoded_payload ble+fsk+css

To start and switch between links, the command sequence is as follows:

  1. sid init <your link(s)>

  2. sid start <your link(s)>

  3. sid stop <your link(s)>

  4. sid deinit

Multiple links can be initialized and started. You have to stop and deinitialize the current link before you can start a new one.

The reset command is used to unregister your device with the cloud. It can only be called on a registered AND time synced device. To unregister, the device needs to send a message to the cloud, so it needs to be synchronized with AWS.

Sidewalk Settings#

To see the available settings commands, enter the following command in the console:

att help

The command-line interface maintains several settings. The Sidewalk settings are distributed in five sections: device, radio, ble, fsk and css. They can be listed by entering:

att get <section name>

The Sidewalk settings are listed with their current state/value. Some of them can be modified by using the following command prototype:

att set <section name>.<setting name> <value>

It is also possible to save your configuration or reset the parameters to their default values with att save and att reset.

sidewalk Section Settings#

Settings in the sidewalk section are directly related to the Sidewalk general state. A detailed setting list can be found below.

Variable

R/W

Type

Values

Description

sidewalk.started_link

R

string

BLE, FSK, CSS, NONE

Currently started link

sidewalk.region

R

string

US

Regulatory domain for Sidewalk

sidewalk.state

R

string

READY, NOT READY, SECURE CHANNEL READY

Device state

sidewalk.time

R

string

"1350808426.972536238"

Gives Endpoint time (GPS time format)

sidewalk.link_connection_policy

RW

string

ml, ac

Link connection policy (multi-link or auto connect)

sidewalk.multi_link_policy

RW

string

def, pow, per, lat, rel

Multi-link policy (default, power save, performance, latency or reliability)

sidewalk.auto_connect_params

RW

string

"<link>, <enabled>, <priority>, <timeout>"

Auto connect parameters (ie: ble,1,10,30 or fsk,0,20,60)

radio Section Settings#

Settings in the radio section are directly related to the Sidewalk radio parameters. A detailed setting list can be found below.

Variable

R

Type

Values

Description

radio.rssi

R

integer

Negative value, for example -30dBm

RSSI from last received message (in dBm)

radio.snr

R

integer

Numeric value, for example 17dB

SNR from last received message (in dB)

⚠ WARNING ⚠: RSSI and SNR values are not valid until at least one message has been received.

ble Section Settings#

The settings in the ble section are directly related to the Sidewalk BLE stack behavior. A detailed setting list can be found below.

Variable

R/W

Type

Values

Description

ble.ble_mtu

R

integer

256

BLE Maximum Transmission Unit in bytes

ble.random_mac

R

string

PUBLIC, RANDOM_PRIVATE_NON_RESOLVABLE, STATIC_RANDOM, RANDOM_PRIVATE_RESOLVABLE

Randomize MAC address

ble.output_power

R

integer

Numeric value, for example 22 for 22dBm

TX output power in dBm

fsk Section Settings#

Settings in the fsk section are directly related to the Sidewalk FSK stack behavior. A detailed setting list can be found below.

Variable

R/W

Type

Values

Description

fsk.data_rate

R

integer

data rate value in Kbps

Current data rate used in FSK in Kbps

fsk.min_freq

R

integer

frequency value in MHz

Start frequency for FSK in MHz

fsk.max_freq

R

integer

frequency value in MHz

Stop frequency for FSK in MHz

fsk.power_profile

R/W

integer

1, 2

Power profile currently in use

fsk.fsk_mtu

R

integer

256

FSK Maximum Transmission Unit in bytes

fsk.rx_window_count

R

integer

INFINITE

Number of RX opportunities (always infinite)

fsk.rx_window_separation

R/W

integer

252

Time between RX opportunities in ms

css Section Settings#

Settings in the css section are directly related to the Sidewalk CSS stack behavior. A detailed setting list can be found below.

Variable

R/W

Type

Values

Description

css.bandwidth

R

integer

bandwidth value in KHz

Current bandwidth used in CSS in kHz

css.min_freq

R

integer

frequency value in MHz

Start frequency for CSS in MHz

css.max_freq

R

integer

frequency value in MHz

Stop frequency for CSS in MHz

css.power_profile

R/W

string

A, B

Power profile currently in use

css.css_mtu

R

integer

256

CSS Maximum Transmission Unit in bytes

css.rx_window_count

R/W

integer

-

Choose the number of RX opportunities

css.rx_window_separation

R/W

integer

-

Time between RX opportunities

⚠ WARNING ⚠: Custom rx_window_separation is not yet supported - only the default 5 seconds is currently accepted.

Interacting with the Cloud#

Gain additional insight on network activity from the cloud perspective by using the techniques described in Getting Started: Interacting with the Cloud.

Report Bugs & Get Support#

You are always encouraged and welcome to ask any questions or report any issues you found to us via Silicon Labs Community.