Testing and Debugging#
RTT Logs#
The UART interface is not always available to report traces from Sidewalk example applications. Instead, reporting leverages the J-Link RTT interface. To set up the communication between your PC and the EFR32, follow these instructions.
Install the J-Link RTT Viewer.
Open the J-Link RTT Viewer.
In the Configuration panel, Connection to J-Link section, select USB.
In the Specify Target Device list, select the connected part (for example EFR32BG21BxxxF1024 or EFR32MG24AxxxF1536).
In the Target Interface & Speed panel, select SWD and 4000 kHz.
In the RTT Control Block panel, select Auto Detection.
Click OK.
Ⓘ INFO Ⓘ: For the KG100S module, select EFR32BG21BxxxF1024 as the target device.
A terminal opens and the Sidewalk application traces are output as shown below (Bluetooth application).
00> [00000001] <I> hello neighbor application started
00> [00000001] <I> sidewalk stack version 1.19.4-20
00> [00000002] <I> silabs sidewalk extension version 2.8.0
02> [00000006] <I> pal kv-storage: kv store opened with 0 object(s)
02> [00000007] <I> pal swi: interrupt init ok
02> [00000008] <W> pal mfg: no objects found in mfg storeBy default, in Amazon Sidewalk sample application, the RTT logs are splitted across 3 terminals:
Terminal 0: Outputs the application logs. They are easy to understand and give basic information on the application status.
Terminal 1: Outputs the Sidewalk stack logs. They are more difficult to understand and require a deep knowledge of the Sidewalk stack. Those logs are in the Amazon Sidewalk stack, the sources are not available.
Terminal 2: Outputs the Sidewalk Platform Abstraction Layer (PAL) logs. They require some knowledge of Sidewalk and can easily be found in the code.
Switch Logs from RTT to UART#
To configure the log output from RTT to UART, follow these steps:
Navigate to Software Components and search for board control. [^1]
In the Board Control component, check if Enable Virtual COM UART is enabled. This is equivalent with:
SL_BOARD_ENABLE_VCOMis defined and it is set to1in theconfig/sl_board_control_config.hfile. [^1]Navigate to Software Components and search for iostream.
Install the IO Stream: USART component (or IO Stream: EUSART for xG28 and xG24).
Access the configuration settings of the newly created VCOM instance called vcom.
If available, disable Enable High frequency mode and enable Restrict the energy mode to allow the reception options.
In
config/sl_cli_config_inst.hchange the value ofSL_CLI_INST_IOSTREAM_HANDLEfromsl_iostream_rtt_handletosl_iostream_vcom_handle. [^2]Navigate back to Software Components and search for sidewalk.
Uninstall the Sidewalk Log: App RTT component and install Sidewalk Log: App VCOM component in its place.
You can also completely remove RTT by replacing Sidewalk Log: PAL RTT and Sidewalk Log: stack RTT by their VCOM equivalent. Then, remove the IO Stream: RTT component.
[^1] These steps do not apply to the KG100S Sidewalk Module Radio Board (BRD4332A) or custom boards.
[^2] This is not required for the Qualification example.
Cloud Application Debugging#
To debug your cloud application, several AWS objects can be use to monitor the events in your account. See Amazon CloudWatch for more information.