Data structure of the user_write_request event.

Public Attributes#

uint8_t
uint8_t
uint16_t

Public Attribute Documentation#

connection#

uint8_t sl_bt_evt_gatt_server_user_write_request_s::connection

Connection handle


characteristic#

uint16_t sl_bt_evt_gatt_server_user_write_request_s::characteristic

GATT characteristic handle. This value is normally received from the gatt_characteristic event.


att_opcode#

uint8_t sl_bt_evt_gatt_server_user_write_request_s::att_opcode

Enum sl_bt_gatt_att_opcode_t. Attribute opcode that informs the procedure from which the value was received.


offset#

uint16_t sl_bt_evt_gatt_server_user_write_request_s::offset

Value offset


value#

byte_array sl_bt_evt_gatt_server_user_write_request_s::value

Value