sl_bt_evt_advertiser_timeout#
Indicates the legacy or extended advertising on an advertising set has stopped because the advertiser has completed the configured number of advertising events or has completed all advertising events that it can perform within the configured duration.
The maximum number of advertising events or advertising duration can be configured by the maxevents or duration parameter in the command sl_bt_advertiser_set_timing.
Modules#
sl_bt_evt_advertiser_timeout_s
Typedefs#
typedef struct sl_bt_evt_advertiser_timeout_s
Macros#
#define
sl_bt_evt_advertiser_timeout_id 0x010400a0
Identifier of the timeout event.