Data structure of the event_info_report event.

Public Attributes#

Public Attribute Documentation#

configuration#

uint32_t sl_bt_evt_linklayer_event_info_report_s::configuration

Bitmask to specify the event info reporting configuration. See the link layer documentation of HCI_VS_Siliconlabs_Event_Info_Reporting_Enable for detailed description of each bit.


procedure_type#

uint8_t sl_bt_evt_linklayer_event_info_report_s::procedure_type

The type of the procedure that is reporting an event. See the link layer documentation of HCI_VS_Siliconlabs_Event_Info_Reporting_Enable for detailed description of available procedure types.


data#

uint8array sl_bt_evt_linklayer_event_info_report_s::data

A variable-length byte array that consists of the following parameters in the specified order:

  • procedure_identifier_length (1 byte)

  • procedure_identifier (procedure_identifier_length * 1 byte)

  • event_info_length (1 byte)

  • event_info (event_info_length * 1 byte)

The length of data must be (2 + procedure_identifier_length + event_info_length) bytes. See the link layer documentation of HCI_VS_Siliconlabs_Event_Info_Report for a detailed description of the parameters.