GATT Descriptor Property Flags#

This enum defines the property flags for GATT characteristic descriptors.

Macros#

#define
SL_BT_GATTDB_DESCRIPTOR_READ 0x1

A GATT client can read the descriptor value.

#define
SL_BT_GATTDB_DESCRIPTOR_WRITE 0x2

A GATT client can write the descriptor value.

#define
SL_BT_GATTDB_DESCRIPTOR_WRITE_NO_RESPONSE 0x4

A GATT client can write the descriptor value without a response.

#define
SL_BT_GATTDB_DESCRIPTOR_LOCAL_ONLY 0x200

The descriptor is local only and should be invisible to GATT clients.