sl_bt_evt_cs_handover_complete#
Indicates that the controller completed the CS handover procedure because synchronization was lost or the configured maximum procedure count was reached.
When this event is sent, the configured CS parameters are removed and the associated connection analyzer handle is deallocated. This event is intended for the CS Follower role.
Modules#
sl_bt_evt_cs_handover_complete_s
Typedefs#
Macros#
#define
sl_bt_evt_cs_handover_complete_id 0x075900a0
Identifier of the handover_complete event.
Typedef Documentation#
sl_bt_evt_cs_handover_complete_t#
typedef struct sl_bt_evt_cs_handover_complete_s sl_bt_evt_cs_handover_complete_t