Data structure of the handover_complete event.

Public Attributes#

uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

reason#

uint8_t sl_bt_evt_cs_handover_complete_s::reason

Enum sl_bt_cs_handover_complete_reason_t. Reason for completion. Values:

  • sl_bt_cs_handover_complete_reason_max_procedure_count_reached (0x0): Configured maximum procedure count was reached.

  • sl_bt_cs_handover_complete_reason_sync_lost (0x1): Synchronization to the connection was lost.


analyzer#

uint8_t sl_bt_evt_cs_handover_complete_s::analyzer

Connection analyzer handle


config_id#

uint8_t sl_bt_evt_cs_handover_complete_s::config_id

CS configuration identifier