Data structure of the result event.

Public Attribute Documentation#

connection#

uint8_t sl_bt_evt_cs_result_s::connection

Connection handle. Returns a SL_BT_INVALID_CONNECTION_HANDLE (0xFF) when triggered as a result of sl_bt_cs_test_start command


config_id#

uint8_t sl_bt_evt_cs_result_s::config_id

CS configuration identifier. This paremeter is ignored when triggered as a result of sl_bt_cs_test_start command.

  • Range: 0 to 3


start_acl_conn_event#

uint16_t sl_bt_evt_cs_result_s::start_acl_conn_event

Starting an ACL connection event count for the results reported in the event. This is reported only in the first subevent in the procedure. For subsequent subevents, this value is set to 0. This parameter is ignored when triggered as a result of sl_bt_cs_test_start command.


procedure_counter#

uint16_t sl_bt_evt_cs_result_s::procedure_counter

Indicates the associated CS procedure count for the results reported in this event. This parameter is ignored when triggered as a result of sl_bt_cs_test_start command.


frequency_compensation#

int16_t sl_bt_evt_cs_result_s::frequency_compensation

Frequency compensation value. Units: 0.01 ppm (15-bit signed integer).

  • Range: -100ppm (-10000) to +100ppm (10000)

  • Value: 0xC000. Frequency compensation value is not available or the role is not initiator. This is reported only in the first subevent in the procedure. For subsequent subevents, this value is set to 0.


reference_power_level#

int8_t sl_bt_evt_cs_result_s::reference_power_level

Reference power level used by the transmission. Units: dBm.

  • Range: -127 to +20

  • Value: 0x07F. The reference power level is not applicable


procedure_done_status#

uint8_t sl_bt_evt_cs_result_s::procedure_done_status

Enum sl_bt_cs_done_status_t. Current status of the CS procedure. Values:

  • sl_bt_cs_done_status_complete (0x0): All results complete for the CS procedure or subevent

  • sl_bt_cs_done_status_partial_results_continue (0x1): Partial results with more to follow

  • sl_bt_cs_done_status_aborted (0xf): Current procedure and all subsequent subevents in the procedure aborted or current subevent aborted.


subevent_done_status#

uint8_t sl_bt_evt_cs_result_s::subevent_done_status

Enum sl_bt_cs_done_status_t. Current status of the CS subevent. Values:

  • sl_bt_cs_done_status_complete (0x0): All results complete for the CS procedure or subevent

  • sl_bt_cs_done_status_partial_results_continue (0x1): Partial results with more to follow

  • sl_bt_cs_done_status_aborted (0xf): Current procedure and all subsequent subevents in the procedure aborted or current subevent aborted.


abort_reason#

uint8_t sl_bt_evt_cs_result_s::abort_reason

Indicates the abort reason when the procedure_done_status or subevent_done_status is set to 0xF, otherwise the default value is set to zero.

Bits 0-3 indicate the procedure abort reasons:

  • 0x0 = Report with no abort

  • 0x1 = Abort because of local Host or remote request

  • 0x2 = Abort because filtered channel map has less than 15 channels

  • 0x3 = Abort because the channel map update instant has passed

  • 0xF = Abort because of unspecified reasons

Bits 4-7 indicate the subevent done reasons:

  • 0x0 = Report with no abort

  • 0x1 = Abort because of local Host or remote request

  • 0x2 = Abort because no CS_SYNC (mode-0) received

  • 0x3 = Abort because of scheduling conflicts or limited resources

  • 0xF = Abort because of unspecified reasons


num_antenna_paths#

uint8_t sl_bt_evt_cs_result_s::num_antenna_paths

Number of antenna paths supported by the local controller for the CS tone exchanges. The number of antenna paths used during the phase measurement stage of the CS step.

  • Range: 1 to 4

  • Value: 0. Phase measurement does not occur during the CS step, therefore ignored


num_steps#

uint8_t sl_bt_evt_cs_result_s::num_steps

Number of steps in the CS subevent for which results are reported.

  • Range: 1 to 160


data#

uint8array sl_bt_evt_cs_result_s::data

The result data is structured as follows:

  • step_mode: 1 octet for each num_steps. Mode type. Range 0 to 3.

  • step_channel: 1 octet for each num_steps. Channel index. Range 1 to 78.

  • step_data_length: 1 octet for each num_steps. Length of mode and role specific information being reported. Range 0x00 to 0xFF.

  • step_data: step_data_length octet for each corresponding steps in num_steps.