Hardware (hardware)#

The commands and events in this class can be used to access and configure the system hardware and peripherals.

hardware commands#

hardware_enable_dcdc#

Deprecated. This command can be used to enable or disable DC/DC.

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x01

lolen

Minimum payload length

2

0x0c

class

Message class:Hardware

3

0x0d

method

Message ID

4

uint8

enable

Set DC/DC as enabled or disabled.

  • 0: disabled

  • 1: enabled

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x02

lolen

Minimum payload length

2

0x0c

class

Message class:Hardware

3

0x0d

method

Message ID

4-5

uint16

result

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes

API#

/* Function */
struct gecko_msg_hardware_enable_dcdc_rsp_t *gecko_cmd_hardware_enable_dcdc(uint8 enable);

/* Response id */
gecko_rsp_hardware_enable_dcdc_id

/* Response structure */
struct gecko_msg_hardware_enable_dcdc_rsp_t
{
  uint16 result
}

hardware_get_time#

Deprecated. Get elapsed time since last reset of RTCC

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x00

lolen

Minimum payload length

2

0x0c

class

Message class:Hardware

3

0x0b

method

Message ID

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x06

lolen

Minimum payload length

2

0x0c

class

Message class:Hardware

3

0x0b

method

Message ID

4-7

uint32

seconds

seconds since last reset

8-9

uint16

ticks

Subsecond ticks of hardware clock, range 0-32767

API#

/* Function */
struct gecko_msg_hardware_get_time_rsp_t *gecko_cmd_hardware_get_time();

/* Response id */
gecko_rsp_hardware_get_time_id

/* Response structure */
struct gecko_msg_hardware_get_time_rsp_t
{
  uint32 seconds,
  uint16 ticks
}

hardware_set_lazy_soft_timer#

This command can be used to start a software timer with some slack. Slack parameter allows stack to optimize wake ups and save power. Timer event is triggered between time and time + slack. See also description of hardware_set_soft_timer command.

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x0a

lolen

Minimum payload length

2

0x0c

class

Message class:Hardware

3

0x0c

method

Message ID

4-7

uint32

time

Interval between how often to send events, in hardware clock ticks (1 second is equal to 32768 ticks). The smallest interval value supported is 328 which is around 10 milliseconds, any parameters between 0 and 328 will be rounded up to 328. The maximum value is 2147483647, which corresponds to about 18.2 hours. If time is 0, removes the scheduled timer with the same handle.

8-11

uint32

slack

Slack time in hardware clock ticks

12

uint8

handle

Timer handle to use, is returned in timeout event

13

uint8

single_shot

Timer mode. Values:

  • 0: false (timer is repeating)

  • 1: true (timer runs only once)

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x02

lolen

Minimum payload length

2

0x0c

class

Message class: Hardware

3

0x0c

method

Message ID

4-5

uint16

result

API#

/* Function */
struct gecko_msg_hardware_set_lazy_soft_timer_rsp_t *gecko_cmd_hardware_set_lazy_soft_timer(uint32 time, uint32 slack, uint8 handle, uint8 single_shot);

/* Response id */
gecko_rsp_hardware_set_lazy_soft_timer_id

/* Response structure */
struct gecko_msg_hardware_set_lazy_soft_timer_rsp_t
{
  uint16 result
}

Events generated#

Event

Description

hardware_soft_timer

Sent after specified interval

hardware_set_soft_timer#

This command can be used to start a software timer. Multiple concurrent timers can be running simultaneously. There are 256 unique timer IDs available. The maximum number of concurrent timers is configurable at device initialization. Up to 16 concurrent timers can be configured. The default configuration is 4. As the RAM for storing timer data is pre-allocated at initialization, an application should not configure the amount more than it needs for minimizing RAM usage.

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x06

lolen

Minimum payload length

2

0x0c

class

Message class:Hardware

3

0x00

method

Message ID

4-7

uint32

time

Interval between how often to send events, in hardware clock ticks (1 second is equal to 32768 ticks). The smallest interval value supported is 328 which is around 10 milliseconds, any parameters between 0 and 328 will be rounded up to 328. The maximum value is 2147483647, which corresponds to about 18.2 hours. If time is 0, removes the scheduled timer with the same handle.

8

uint8

handle

Timer handle to use, is returned in timeout event

9

uint8

single_shot

Timer mode. Values:

  • 0: false (timer is repeating)

  • 1: true (timer runs only once)

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x02

lolen

Minimum payload length

2

0x0c

class

Message class:Hardware

3

0x00

method

Message ID

4-5

uint16

result

API#

/* Function */
struct gecko_msg_hardware_set_soft_timer_rsp_t *gecko_cmd_hardware_set_soft_timer(uint32 time, uint8 handle, uint8 single_shot);

/* Response id */
gecko_rsp_hardware_set_soft_timer_id

/* Response structure */
struct gecko_msg_hardware_set_soft_timer_rsp_t
{
  uint16 result
}

Events generated#

Event

Description

hardware_soft_timer

Sent after specified interval

hardware events#

hardware_soft_timer#

This event indicates that the soft timer has lapsed.

Event#

Byte

Type

Name

Description

0

0xa0

hilen

Message type: Event

1

0x01

lolen

Minimum payload length

2

0x0c

class

Message class:Hardware

3

0x00

method

Message ID

4

uint8

handle

Timer Handle

API#

/* event id*/
gecko_evt_hardware_soft_timer_id

/* event structure*/
struct gecko_msg_hardware_soft_timer_evt_t
{
  uint8 handle
}