testing commands (test)#

test commands#

test_dtm_end#

This command can be used to end a transmitter or a receiver test. When the command is processed by the radio and the test has ended, a test_dtm_completed event is triggered.

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x00

lolen

Minimum payload length

2

0x0e

class

Message class:testing commands

3

0x02

method

Message ID

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x02

lolen

Minimum payload length

2

0x0e

class

Message class:testing commands

3

0x02

method

Message ID

4-5

uint16

result

Command result

API#

/* Function */
struct gecko_msg_test_dtm_end_rsp_t *gecko_cmd_test_dtm_end();

/* Response id */
gecko_rsp_test_dtm_end_id

/* Response structure */
struct gecko_msg_test_dtm_end_rsp_t
{
  uint16 result
}

Events generated#

Event

Description

test_dtm_completed

This event is received when the command is processed.

test_dtm_rx#

This command can be used to start a receiver test. The test is meant to be used against a separate Bluetooth tester device. When the command is processed by the radio, a test_dtm_completed event is triggered. This event indicates if the test started successfully.

Parameter phy specifies which PHY is used to receive the packets. All devices support at least the 1M PHY.

The test may be stopped using the test_dtm_end command. This will trigger another test_dtm_completed event, which carries the number of packets received during the test.

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x02

lolen

Minimum payload length

2

0x0e

class

Message class:testing commands

3

0x01

method

Message ID

4

uint8

channel

Bluetooth channel

Range: 0-39

Channel is (F - 2402) / 2, where F is frequency in MHz

5

uint8

phy

PHY to use

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x02

lolen

Minimum payload length

2

0x0e

class

Message class:testing commands

3

0x01

method

Message ID

4-5

uint16

result

Command result

API#

/* Function */
struct gecko_msg_test_dtm_rx_rsp_t *gecko_cmd_test_dtm_rx(uint8 channel, uint8 phy);

/* Response id */
gecko_rsp_test_dtm_rx_id

/* Response structure */
struct gecko_msg_test_dtm_rx_rsp_t
{
  uint16 result
}

Events generated#

Event

Description

test_dtm_completed

This event is received when the command is processed.

test_dtm_tx#

This command can be used to start a transmitter test. The test is meant to be used against a separate Bluetooth tester device. When the command is processed by the radio, a test_dtm_completed event is triggered. This event indicates if the test started successfully.

In the transmitter test, the device sends packets continuously with a fixed interval. The type and length of each packet is set by packet_type and length parameters. Parameter phy specifies which PHY is used to transmit the packets. All devices support at least the 1M PHY. There is also a special packet type, test_pkt_carrier , which can be used to transmit continuous unmodulated carrier. The length field is ignored in this mode.

The test may be stopped using the test_dtm_end command.

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x04

lolen

Minimum payload length

2

0x0e

class

Message class:testing commands

3

0x00

method

Message ID

4

uint8

packet_type

Packet type to transmit

5

uint8

length

Packet length in bytes

Range: 0-255

6

uint8

channel

Bluetooth channel

Range: 0-39

Channel is (F - 2402) / 2, where F is frequency in MHz

7

uint8

phy

PHY to use

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x02

lolen

Minimum payload length

2

0x0e

class

Message class:testing commands

3

0x00

method

Message ID

4-5

uint16

result

Command result

API#

/* Function */
struct gecko_msg_test_dtm_tx_rsp_t *gecko_cmd_test_dtm_tx(uint8 packet_type, uint8 length, uint8 channel, uint8 phy);

/* Response id */
gecko_rsp_test_dtm_tx_id

/* Response structure */
struct gecko_msg_test_dtm_tx_rsp_t
{
  uint16 result
}

Events generated#

Event

Description

test_dtm_completed

This event is received when the command is processed.

test events#

test_dtm_completed#

This event indicates that the radio has processed a test start or end command. The result parameter indicates the success of the command.

After the receiver or transmitter test is stopped, the number_of_packets parameter in this event indicates the number of received or transmitted packets.

Event#

Byte

Type

Name

Description

0

0xa0

hilen

Message type: Event

1

0x04

lolen

Minimum payload length

2

0x0e

class

Message class:testing commands

3

0x00

method

Message ID

4-5

uint16

result

Command result

6-7

uint16

number_of_packets

Number of packets only valid for test_dtm_end command.

API#

/* event id*/
gecko_evt_test_dtm_completed_id

/* event structure*/
struct gecko_msg_test_dtm_completed_evt_t
{
  uint16 result,
  uint16 number_of_packets
}

test enumerations#

test_packet_type#

Test packet types

Number 3 corresponding to unmodulated carrier packet type is deprecated. Valid number is 254.

Enumerations#

Value

Name

Description

0

test_pkt_prbs9

PRBS9 packet payload

1

test_pkt_11110000

11110000 packet payload

2

test_pkt_10101010

10101010 packet payload

3

test_pkt_carrier_deprecated

Unmodulated carrier - deprecated

4

test_pkt_11111111

11111111 packet payload

5

test_pkt_00000000

00000000 packet payload

6

test_pkt_00001111

00001111 packet payload

7

test_pkt_01010101

01010101 packet payload

253

test_pkt_pn9

PN9 continuously modulated output

254

test_pkt_carrier

Unmodulated carrier

test_phy#

Test PHY types

Enumerations#

Value

Name

Description

1

test_phy_1m

1M PHY

2

test_phy_2m

2M PHY

3

test_phy_125k

125k Coded PHY

4

test_phy_500k

500k Coded PHY