CTE Transmitter (cte_transmitter)#

Commands and events in this class can be used to manage Constant Tone Extension (CTE) transmission.

CTE feature is only supported by specific devices. Commands from this class will return bg_err_not_supported on devices that do not support CTE.

cte_transmitter commands#

cte_transmitter_clear_dtm_parameters#

This command can be used to clear CTE related parameters that were previously set for LE transmitter test. Default values will be restored for these parameters.

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x00

lolen

Minimum payload length

2

0x44

class

Message class:CTE Transmitter

3

0x05

method

Message ID

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x02

lolen

Minimum payload length

2

0x44

class

Message class:CTE Transmitter

3

0x05

method

Message ID

4-5

uint16

result

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes

API#

/* Function */
struct gecko_msg_cte_transmitter_clear_dtm_parameters_rsp_t *gecko_cmd_cte_transmitter_clear_dtm_parameters();

/* Response id */
gecko_rsp_cte_transmitter_clear_dtm_parameters_id

/* Response structure */
struct gecko_msg_cte_transmitter_clear_dtm_parameters_rsp_t
{
  uint16 result
}

cte_transmitter_disable_cte_response#

This command can be used to disable CTE responses on a connection.

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x01

lolen

Minimum payload length

2

0x44

class

Message class:CTE Transmitter

3

0x01

method

Message ID

4

uint8

connection

Connection handle

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x02

lolen

Minimum payload length

2

0x44

class

Message class:CTE Transmitter

3

0x01

method

Message ID

4-5

uint16

result

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes

API#

/* Function */
struct gecko_msg_cte_transmitter_disable_cte_response_rsp_t *gecko_cmd_cte_transmitter_disable_cte_response(uint8 connection);

/* Response id */
gecko_rsp_cte_transmitter_disable_cte_response_id

/* Response structure */
struct gecko_msg_cte_transmitter_disable_cte_response_rsp_t
{
  uint16 result
}

cte_transmitter_enable_cte_response#

This command can be used to enable CTE responses on a connection.

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x03

lolen

Minimum payload length

2

0x44

class

Message class:CTE Transmitter

3

0x00

method

Message ID

4

uint8

connection

Connection handle

5

uint8

cte_types

CTE types. Bitmask of followings,

  • Bit 0: AoA CTE response

  • Bit 1: AoD CTE response with 1us slots

  • Bit 2: AoD CTE response with 2us slots

6

uint8array

switching_pattern

Antenna switching pattern

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x02

lolen

Minimum payload length

2

0x44

class

Message class:CTE Transmitter

3

0x00

method

Message ID

4-5

uint16

result

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes

API#

/* Function */
struct gecko_msg_cte_transmitter_enable_cte_response_rsp_t *gecko_cmd_cte_transmitter_enable_cte_response(uint8 connection, uint8 cte_types, uint8 switching_pattern_len, const uint8 *switching_pattern_data);

/* Response id */
gecko_rsp_cte_transmitter_enable_cte_response_id

/* Response structure */
struct gecko_msg_cte_transmitter_enable_cte_response_rsp_t
{
  uint16 result
}

cte_transmitter_set_dtm_parameters#

This command can be used to set CTE related parameters of LE transmitter test.

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x03

lolen

Minimum payload length

2

0x44

class

Message class:CTE Transmitter

3

0x04

method

Message ID

4

uint8

cte_length

Expected length of the Constant Tone Extension in 8 us units

5

uint8

cte_type

CTE type

  • 0: AoA CTE

  • 1: AoD CTE with 1 us slots

  • 2: AoD CTE with 2 us slots

6

uint8array

switching_pattern

Antenna switching pattern

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x02

lolen

Minimum payload length

2

0x44

class

Message class:CTE Transmitter

3

0x04

method

Message ID

4-5

uint16

result

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes(error-codes)

API#

/* Function */
struct gecko_msg_cte_transmitter_set_dtm_parameters_rsp_t *gecko_cmd_cte_transmitter_set_dtm_parameters(uint8 cte_length, uint8 cte_type, uint8 switching_pattern_len, const uint8 *switching_pattern_data);

/* Response id */
gecko_rsp_cte_transmitter_set_dtm_parameters_id

/* Response structure */
struct gecko_msg_cte_transmitter_set_dtm_parameters_rsp_t
{
  uint16 result
}