CTE Receiver (cte_receiver)#
Commands and events in this class can be used to manage Constant Tone Extension (CTE) receiving.
CTE feature is only supported by specific devices. Commands from this class will return bg_err_not_supported on devices that do not support CTE.
cte_receiver commands#
cte_receiver_clear_dtm_parameters#
This command can be used to clear CTE related parameters that were previously set for LE receiver test. Default values will be restored for these parameters.
Command#
Byte | Type | Name | Description |
|---|---|---|---|
0 | 0x20 | hilen | Message type: Command |
1 | 0x00 | lolen | Minimum payload length |
2 | 0x45 | class | Message class:CTE Receiver |
3 | 0x06 | method | Message ID |
Response#
Byte | Type | Name | Description |
|---|---|---|---|
0 | 0x20 | hilen | Message type: Response |
1 | 0x02 | lolen | Minimum payload length |
2 | 0x45 | class | Message class:CTE Receiver |
3 | 0x06 | method | Message ID |
4-5 | uint16 | result | Result code
|
API#
/* Function */
struct gecko_msg_cte_receiver_clear_dtm_parameters_rsp_t *gecko_cmd_cte_receiver_clear_dtm_parameters();
/* Response id */
gecko_rsp_cte_receiver_clear_dtm_parameters_id
/* Response structure */
struct gecko_msg_cte_receiver_clear_dtm_parameters_rsp_t
{
uint16 result
}cte_receiver_set_dtm_parameters#
This command can be used to set CTE related parameters of LE receiver test.
Command#
Byte | Type | Name | Description |
|---|---|---|---|
0 | 0x20 | hilen | Message type: Command |
1 | 0x04 | lolen | Minimum payload length |
2 | 0x45 | class | Message class:CTE Receiver |
3 | 0x05 | method | Message ID |
4 | uint8 | cte_length | Expected length of the Constant Tone Extension in 8 us units |
5 | uint8 | cte_type | Expected CTE type
|
6 | uint8 | slot_durations | Slot durations
|
7 | uint8array | switching_pattern | Antenna switching pattern |
Response#
Byte | Type | Name | Description |
|---|---|---|---|
0 | 0x20 | hilen | Message type: Response |
1 | 0x02 | lolen | Minimum payload length |
2 | 0x45 | class | Message class:CTE Receiver |
3 | 0x05 | method | Message ID |
4-5 | uint16 | result | Result code
|
API#
/* Function */
struct gecko_msg_cte_receiver_set_dtm_parameters_rsp_t *gecko_cmd_cte_receiver_set_dtm_parameters(uint8 cte_length, uint8 cte_type, uint8 slot_durations, uint8 switching_pattern_len, const uint8 *switching_pattern_data);
/* Response id */
gecko_rsp_cte_receiver_set_dtm_parameters_id
/* Response structure */
struct gecko_msg_cte_receiver_set_dtm_parameters_rsp_t
{
uint16 result
}cte_receiver_start_iq_sampling#
This command can be used to start IQ samplings on a connection.
Command#
Byte | Type | Name | Description |
|---|---|---|---|
0 | 0x20 | hilen | Message type: Command |
1 | 0x07 | lolen | Minimum payload length |
2 | 0x45 | class | Message class:CTE Receiver |
3 | 0x01 | method | Message ID |
4 | uint8 | connection | Connection handle |
5-6 | uint16 | interval | Measurement interval
|
7 | uint8 | cte_length | Minimum length of the CTE being requested in 8 us units |
8 | uint8 | cte_type | Requested CTE type
|
9 | uint8 | slot_durations | Slot durations
|
10 | uint8array | switching_pattern | Antenna switching pattern |
Response#
Byte | Type | Name | Description |
|---|---|---|---|
0 | 0x20 | hilen | Message type: Response |
1 | 0x02 | lolen | Minimum payload length |
2 | 0x45 | class | Message class:CTE Receiver |
3 | 0x01 | method | Message ID |
4-5 | uint16 | result | Result code
|
API#
/* Function */
struct gecko_msg_cte_receiver_start_iq_sampling_rsp_t *gecko_cmd_cte_receiver_start_iq_sampling(uint8 connection, uint16 interval, uint8 cte_length, uint8 cte_type, uint8 slot_durations, uint8 switching_pattern_len, const uint8 *switching_pattern_data);
/* Response id */
gecko_rsp_cte_receiver_start_iq_sampling_id
/* Response structure */
struct gecko_msg_cte_receiver_start_iq_sampling_rsp_t
{
uint16 result
}Events generated#
Event | Description |
|---|---|
cte_receiver_iq_report | Triggered when IQ samples have been received. |
cte_receiver_stop_iq_sampling#
This command can be used to stop the IQ sampling on a connection.
Command#
Byte | Type | Name | Description |
|---|---|---|---|
0 | 0x20 | hilen | Message type: Command |
1 | 0x01 | lolen | Minimum payload length |
2 | 0x45 | class | Message class:CTE Receiver |
3 | 0x02 | method | Message ID |
4 | uint8 | connection | Connection handle |
Response#
Byte | Type | Name | Description |
|---|---|---|---|
0 | 0x20 | hilen | Message type: Response |
1 | 0x02 | lolen | Minimum payload length |
2 | 0x45 | class | Message class:CTE Receiver |
3 | 0x02 | method | Message ID |
4-5 | uint16 | result | Result code
|
API#
/* Function */
struct gecko_msg_cte_receiver_stop_iq_sampling_rsp_t *gecko_cmd_cte_receiver_stop_iq_sampling(uint8 connection);
/* Response id */
gecko_rsp_cte_receiver_stop_iq_sampling_id
/* Response structure */
struct gecko_msg_cte_receiver_stop_iq_sampling_rsp_t
{
uint16 result
}cte_receiver events#
cte_receiver_iq_report#
IQ samples report from connection or connectionless CTE packets.
Event#
Byte | Type | Name | Description |
|---|---|---|---|
0 | 0xa0 | hilen | Message type: Event |
1 | 0x0d | lolen | Minimum payload length |
2 | 0x45 | class | Message class:CTE Receiver |
3 | 0x00 | method | Message ID |
4-5 | uint16 | status | Status of CTE IQ sampling |
6 | uint8 | packet_type | CTE packet type
|
7 | uint8 | handle | Connection handle or periodic advertising synchronization handle |
8 | uint8 | phy | The PHY on which the packet is received on a connection. Ingore this field for connectionless IQ reports.
|
9 | uint8 | channel | The channel on which the CTE packet was received |
10 | int8 | rssi | RSSI in the received CTE packet. Unit: dBm |
11 | uint8 | rssi_antenna_id | The ID of the antenna on which RSSI was measured |
12 | uint8 | cte_type | The CTE type
|
13 | uint8 | slot_durations | Slot durations
|
14-15 | uint16 | event_counter | The event counter of the periodic advertising train or the connection |
16 | uint8array | samples | IQ samples in received CTE packet |
API#
/* event id*/
gecko_evt_cte_receiver_iq_report_id
/* event structure*/
struct gecko_msg_cte_receiver_iq_report_evt_t
{
uint16 status,
uint8 packet_type,
uint8 handle,
uint8 phy,
uint8 channel,
int8 rssi,
uint8 rssi_antenna_id,
uint8 cte_type,
uint8 slot_durations,
uint16 event_counter,
uint8array samples
}