Persistent Store (flash)#

Persistent Store commands can be used to manage user data in PS keys in the flash memory of the Bluetooth device. User data stored within the flash memory is persistent across reset and power cycling of the device. The persistent store size is 2048 bytes. As Bluetooth bondings are also stored in this area, the space available for user data additionally depends on the number of bondings the device has at the time. The size of a Bluetooth bonding is around 150 bytes.

The maximum user data size associated to a PS key is 56 bytes.

flash commands#

flash_ps_erase#

This command can be used to erase a single PS key and its value from the persistent store.

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x02

lolen

Minimum payload length

2

0x0d

class

Message class:Persistent Store

3

0x04

method

Message ID

4-5

uint16

key

PS key to erase

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x02

lolen

Minimum payload length

2

0x0d

class

Message class:Persistent Store

3

0x04

method

Message ID

4-5

uint16

result

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes(error-codes)

API#

/* Function */
struct gecko_msg_flash_ps_erase_rsp_t *gecko_cmd_flash_ps_erase(uint16 key);

/* Response id */
gecko_rsp_flash_ps_erase_id

/* Response structure */
struct gecko_msg_flash_ps_erase_rsp_t
{
  uint16 result
}

flash_ps_erase_all#

This command can be used to erase all PS keys and their corresponding values.

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x00

lolen

Minimum payload length

2

0x0d

class

Message class:Persistent Store

3

0x01

method

Message ID

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x02

lolen

Minimum payload length

2

0x0d

class

Message class:Persistent Store

3

0x01

method

Message ID

4-5

uint16

result

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes(error-codes)

API#

/* Function */
struct gecko_msg_flash_ps_erase_all_rsp_t *gecko_cmd_flash_ps_erase_all();

/* Response id */
gecko_rsp_flash_ps_erase_all_id

/* Response structure */
struct gecko_msg_flash_ps_erase_all_rsp_t
{
  uint16 result
}

flash_ps_load#

This command can be used for retrieving the value of the specified PS key.

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x02

lolen

Minimum payload length

2

0x0d

class

Message class:Persistent Store

3

0x03

method

Message ID

4-5

uint16

key

PS key of the value to be retrieved

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x03

lolen

Minimum payload length

2

0x0d

class

Message class:Persistent Store

3

0x03

method

Message ID

4-5

uint16

result

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes(error-codes)

6

uint8array

value

The returned value of the specified PS key.

API#

/* Function */
struct gecko_msg_flash_ps_load_rsp_t *gecko_cmd_flash_ps_load(uint16 key);

/* Response id */
gecko_rsp_flash_ps_load_id

/* Response structure */
struct gecko_msg_flash_ps_load_rsp_t
{
  uint16 result,
  uint8array value
}

flash_ps_save#

This command can be used to store a value into the specified PS key. Allowed PS keys are in range from 0x4000 to 0x407F. At most 56 bytes user data can be stored in one PS key. Error code 0x018a (command_too_long) will be returned if more than 56 bytes data is passed in.

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x03

lolen

Minimum payload length

2

0x0d

class

Message class:Persistent Store

3

0x02

method

Message ID

4-5

uint16

key

PS key

6

uint8array

value

Value to store into the specified PS key.

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x02

lolen

Minimum payload length

2

0x0d

class

Message class:Persistent Store

3

0x02

method

Message ID

4-5

uint16

result

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes(error-codes)

API#

/* Function */
struct gecko_msg_flash_ps_save_rsp_t *gecko_cmd_flash_ps_save(uint16 key, uint8 value_len, const uint8 *value_data);

/* Response id */
gecko_rsp_flash_ps_save_id

/* Response structure */
struct gecko_msg_flash_ps_save_rsp_t
{
  uint16 result
}