sl_bt_evt_sync_closedSynchronization#

Indicates that periodic advertising synchronization was lost or a synchronization establishment procedure was canceled.

Data Structures#

struct  

sl_bt_evt_sync_closed_s

Data structure of the closed event.

Macros#

#define

sl_bt_evt_sync_closed_id

0x014200a0

Identifier of the closed event.

Detailed Description#

Indicates that periodic advertising synchronization was lost or a synchronization establishment procedure was canceled.

The synchronization establishment procedure can be cancelled explicitly by the application by issuing command sl_bt_sync_close, or internally due to synchronization failing. Synchronization can fail for example due to incompatible sync CTE type.

Data Structure Documentation#

sl_bt_evt_sync_closed_s#

struct sl_bt_evt_sync_closed_s

Data structure of the closed event.

Data Fields

uint16_t

reason

  • Result code 0: success

  • Non-zero: an error has occurred

uint16_t

sync

Periodic advertising synchronization handle