sl_bt_evt_sync_dataSynchronization#
Reports a received periodic advertisement packet.
Data Structures#
struct | |
Data structure of the data event. |
Macros#
define | sl_bt_evt_sync_data_id 0x024200a0 |
Identifier of the data event. |
Detailed Description#
Reports a received periodic advertisement packet.
Data Structure Documentation#
sl_bt_evt_sync_data_s#
struct sl_bt_evt_sync_data_s |
Data structure of the data event.
Data Fields | ||
|---|---|---|
uint16_t | sync | Periodic advertising synchronization handle |
int8_t | tx_power | TX power value in the received packet header.
|
int8_t | rssi | Signal strength indicator (RSSI) in the latest received packet. Units: dBm* Range: -127 to +20 |
uint8_t | data_status |
|
data | Periodic advertising data |