sl_bt_evt_sync_openedSynchronization#

Indicates that a periodic advertising synchronization has been opened.

Data Structures#

struct  

sl_bt_evt_sync_opened_s

Data structure of the opened event.

Macros#

#define

sl_bt_evt_sync_opened_id

0x004200a0

Identifier of the opened event.

Detailed Description#

Indicates that a periodic advertising synchronization has been opened.

Data Structure Documentation#

sl_bt_evt_sync_opened_s#

struct sl_bt_evt_sync_opened_s

Data structure of the opened event.

Data Fields

uint16_t

sync

Periodic advertising synchronization handle

uint8_t

adv_sid

Advertising set identifier

bd_addr

address

Address of the advertiser

uint8_t

address_type

Advertiser address type. Values:

  • 0: Public address

  • 1: Random address

uint8_t

adv_phy

Enum gap_phy_type_t. The advertiser PHY. Values:

  • gap_1m_phy (0x1):** 1M PHY

  • gap_2m_phy (0x2): 2M PHY

  • gap_coded_phy (0x4): Coded PHY

uint16_t

adv_interval

The periodic advertising interval.

  • Value in units of 1.25 ms

  • Range: 0x06 to 0xFFFF

  • Time range: 7.5 ms to 81.92 s

uint16_t

clock_accuracy

Enum sync_advertiser_clock_accuracy_t. The advertiser clock accuracy.

uint8_t

bonding

Bonding handle.

  • Values: SL_BT_INVALID_BONDING_HANDLE (0xff): No bonding

  • Other: Bonding handle