byte_array Struct Reference#
Variable-length int8_t array.
#include <sl_bt_types.h>
Data Fields#
uint16_t | |
int8_t | data [] |
Variable-length int8_t array.
Field Documentation#
len#
uint16\_t byte\_array::lenNumber of bytes stored in data
data#
int8\_t byte\_array::data[]Data bytes
The documentation for this struct was generated from the following file:
inc/
sl_bt_types.h