sl_bt_evt_connection_closedConnection#
Indicates that a connection was closed.
Data Structures#
struct | Data structure of the closed event. |
Macros#
# define | sl_bt_evt_connection_closed_id 0x010600a0 Identifier of the closed event. |
Detailed Description#
Indicates that a connection was closed.
Data Structure Documentation#
◆ sl_bt_evt_connection_closed_s#
struct sl_bt_evt_connection_closed_s#
Data structure of the closed event.
Data Fields
uint16_t | reason | Reason of connection close |
uint8_t | connection | Handle of the closed connection |