sl_bt_evt_connection_rssiConnection#

Triggered when an connection_get_rssi command has completed.

Data Structures#


struct | sl_bt_evt_connection_rssi_s | Data structure of the rssi event.

Macros#


define | sl_bt_evt_connection_rssi_id 0x030600a0#

| Identifier of the rssi event.

Detailed Description#

Triggered when an connection_get_rssi command has completed.


Data Structure Documentation#

◆ sl_bt_evt_connection_rssi_s#

struct sl_bt_evt_connection_rssi_s#

Data structure of the rssi event.

Data Fields#

uint8_t | connection |

Connection handle

uint8_t | status |

Command complete status:

  • 0x00: The command succeeded

  • 0x01-0xFF: The command failed. See Bluetooth Core specification v5.0 [Vol 2] Part D, Error Codes

int8_t | rssi |

The median of the last seven measured RSSI values on the connection. Units: dBm. Range: -127 to +20. Ignore this parameter if the command fails.